SGTL5000 CPFILT on 20-pin QFN package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SGTL5000 CPFILT on 20-pin QFN package

ソリューションへジャンプ
822件の閲覧回数
jaydcarlson
Contributor III

Regarding the SGTL5000 datasheet, on page 4, Table 1, it lists that the CPFILT must be installed if VDDIO and VDDA are both < 3.0V (which is true in our case – VDDA=2.5V, VDDIO=1.8V). But we’re using the 20-pin package, and it doesn’t break out the CPFILT pin.

Does the 20-pin QFN version of the SGTL5000 not support VDDA = 2.5, VDDIO = 1.8V?

0 件の賞賛
返信
1 解決策
686件の閲覧回数
art
NXP Employee
NXP Employee

Since the CPFILT pin is missing on the 20-pin QFN package, the internal charge pump becomes non-functional. So, the SGTL5000 parts in 20-pin package cannot support the applications where both VDDA and VDDIO are less than 3.0V .


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
687件の閲覧回数
art
NXP Employee
NXP Employee

Since the CPFILT pin is missing on the 20-pin QFN package, the internal charge pump becomes non-functional. So, the SGTL5000 parts in 20-pin package cannot support the applications where both VDDA and VDDIO are less than 3.0V .


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信