SGTL5000 CPFILT on 20-pin QFN package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGTL5000 CPFILT on 20-pin QFN package

Jump to solution
665 Views
jaydcarlson
Contributor III

Regarding the SGTL5000 datasheet, on page 4, Table 1, it lists that the CPFILT must be installed if VDDIO and VDDA are both < 3.0V (which is true in our case – VDDA=2.5V, VDDIO=1.8V). But we’re using the 20-pin package, and it doesn’t break out the CPFILT pin.

Does the 20-pin QFN version of the SGTL5000 not support VDDA = 2.5, VDDIO = 1.8V?

0 Kudos
1 Solution
529 Views
art
NXP Employee
NXP Employee

Since the CPFILT pin is missing on the 20-pin QFN package, the internal charge pump becomes non-functional. So, the SGTL5000 parts in 20-pin package cannot support the applications where both VDDA and VDDIO are less than 3.0V .


Have a great day,
Artur
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
530 Views
art
NXP Employee
NXP Employee

Since the CPFILT pin is missing on the 20-pin QFN package, the internal charge pump becomes non-functional. So, the SGTL5000 parts in 20-pin package cannot support the applications where both VDDA and VDDIO are less than 3.0V .


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos