Hi Brat,
You can see that in our Android_Release_Notes.pdf you can see that the default board support the follow :
Connectivity - BT
Hardware:
• Silex AR6233X SDIO card
About the AR6210 in default BSP do not have the drive or SDK, you can contact your BlueTooth vendor for help.
NXP BSP was only verified with Silex AR6233X bluetooth, and th HAL code was got from bluetooth vendor.
The customer should also get the HAL code and Android porting document from their BlueTooth vendor. It is not same as Silex AR6233X.
And there are some useful threads you can refer to:
How to enable BT on board imx6q_sabresd RevC.
USB Bluetooth Dongle not working
Hope this can help you.
Have a great day,
(Dan)
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Brat,
It's my pleasure:smileyhappy:.
Have a nice day
Best Regards
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------