Hi,
We're working with an i.MX 6 series SABRE board and had a question regarding the included JTAG adapter. We're trying to locate a schematic for the adapter so we can see what the pin assignments are. We've got the schematics for the CPU card but have not had any luck in locating one for the adapter. Is one available? Thanks.
Hello,
The i.MX6 provides standard JTAG interface, that may be used either
for Boundary Scan (IEEE1149.1) or for software JTAG debugging.
Please refer to i.MX6 Reference Manual(s) for more details about
the JTAG interface. NXP / FSL designs use standard (20-pin) connector
for it, which is intended for external Emulators/Probes.
Please look at corresponding section of the i.MX6 Design tool Web :
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------