Hello,
is there a possibility to change the pinmuxing at runtime. I need to do a very slow squence (5 Baud) on a UART interface. The simpliest thing would be using GPIO operations on the Tx Pin of the UART. Is there a possibility to change the pinmux settings without a reboot?
Thanks!
/Robert
解決済! 解決策の投稿を見る。
Hi Robert,
There are some ways to change the pin functions on runtime from Linux. One option could be using the Memtool, which is already included in our BPSs; please refer to the following thread for additional details:
Other option could be use the Devregs. You could get additional details on the following Community document:
devregs - tool to display and modify a device's registers at runtime
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Carlos,
thank you for your reply. I used the memtool and it does the job for me.
Best regards
~Robert
Hi Robert,
There are some ways to change the pin functions on runtime from Linux. One option could be using the Memtool, which is already included in our BPSs; please refer to the following thread for additional details:
Other option could be use the Devregs. You could get additional details on the following Community document:
devregs - tool to display and modify a device's registers at runtime
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------