Regarding the display used on the SABRE-SD board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding the display used on the SABRE-SD board

ソリューションへジャンプ
701件の閲覧回数
patcharasirigul
Contributor II

Hello everyone,

We're planning to use display for connecting with SABRE board, but we're looking for another display to use with it. The type of interface we use is LVDS. I've read the datasheet of display the SABRE board used is : http://boundarydevices.com/wp-content/uploads/2013/06/HSD100PXN1-A00-C11-1.0.pdf

I found the pin assignment on page 13. The pin 4, pin 6 and pin 7 are V_EDID, CLK_EDID and DATA_EDID. but the display we are planning to use, it does't have these pin.

I'd like to know what the pin 4, 6 and 7 is.

Can I connect the another display without pin 4, 6 and 7 ?

and What is the effect if I connect the display without these pin ?

Please help me.

Thank you so much.

ラベル(3)
0 件の賞賛
返信
1 解決策
636件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Patchara

this particular HannStar lvds LCD has i2c ID data for identification

(similar to hdmi monitors). Not all lvds LCDs has such ID signals and it is

not used in BSP. You can any use suitable lvds LCD without these signals.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
637件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Patchara

this particular HannStar lvds LCD has i2c ID data for identification

(similar to hdmi monitors). Not all lvds LCDs has such ID signals and it is

not used in BSP. You can any use suitable lvds LCD without these signals.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信