Hi All,
I tried to download the git respository for qt4.8, but getting the following error...
git clone http://git.gitorious.org/qt/qt.git qt
Initialized empty Git repository in /home/vishva/qt/.git/
remote: Counting objects: 738088, done
remote: Finding sources: 100% (738088/738088)
remote: Compressing objects: 100% (109395/109395)
remote: Compressing objects: 100% (108833/108833)
error: RPC failed; result=18, HTTP code = 20056 MiB | 42 KiB/s
Any suggestions or alternate source??
You can turn trace and verbose on for GIT to see what's going on:
$ export GIT_TRACE=1
$ export GIT_CURL_VERBOSE=1
$ git clone http://git.gitorious.org/qt/qt.git qt
Thanks. After trying for a couple of more times i was able to download.. but getting the following error for STEP #7.
./configure -qpa -arch arm -xplatform qws/linux-imx6-g++ -no-largefile -no-accessibility -opensource -verbose -system-libpng -system-libjpeg -system-freetype -fast -opengl es2 -egl -confirm-license -qt-zlib -qt-libpng -no-webkit -no-multimedia -make examples -make demos -release -make libs -exceptions -no-qt3support -prefix /opt/qt4/
Determining system architecture... (Linux:2.6.32-50-generic:i686)
32-bit Intel 80x86 (i386)
'arm' is supported
'i386' is supported
System architecture: 'arm'
Host architecture: 'i386'
Precompiled-headers support enabled.
Symbol visibility control enabled.
This is the Qt Lighthouse Open Source Edition.
You are licensed to use this software under the terms of
the Lesser GNU General Public License (LGPL) versions 2.1.
You have already accepted the terms of the license.
header created for /home/vishva/qt/src/corelib/global/qconfig.h (1)
Creating qmake. Please wait...
make: Nothing to be done for `first'.
You have not explicitly asked to use pkg-config and are cross-compiling.
pkg-config will not be used to automatically query cflag/lib parameters for
dependencies
floatmath auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o floatmath.o floatmath.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [floatmath.o] Error 1
floatmath disabled.
mmx auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -mmmx -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o mmx.o mmx.cpp
cc1plus: error: unrecognized command line option '-mmmx'
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [mmx.o] Error 1
mmx disabled.
3dnow auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -m3dnow -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o 3dnow.o 3dnow.cpp
cc1plus: error: unrecognized command line option '-m3dnow'
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [3dnow.o] Error 1
3dnow disabled.
sse auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -msse -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o sse.o sse.cpp
cc1plus: error: unrecognized command line option '-msse'
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [sse.o] Error 1
sse disabled.
sse2 auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -msse2 -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o sse2.o sse2.cpp
cc1plus: error: unrecognized command line option '-msse2'
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [sse2.o] Error 1
sse2 disabled.
sse3 auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -msse3 -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o sse3.o sse3.cpp
cc1plus: error: unrecognized command line option '-msse3'
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [sse3.o] Error 1
sse3 disabled.
ssse3 auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -mssse3 -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o ssse3.o ssse3.cpp
cc1plus: error: unrecognized command line option '-mssse3'
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [ssse3.o] Error 1
ssse3 disabled.
sse4_1 auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -msse4.1 -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o sse4_1.o sse4_1.cpp
cc1plus: error: unrecognized command line option '-msse4.1'
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [sse4_1.o] Error 1
sse4_1 disabled.
sse4_2 auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -msse4.2 -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o sse4_2.o sse4_2.cpp
cc1plus: error: unrecognized command line option '-msse4.2'
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [sse4_2.o] Error 1
sse4_2 disabled.
avx auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -mavx -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o avx.o avx.cpp
cc1plus: error: unrecognized command line option '-mavx'
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [avx.o] Error 1
avx disabled.
neon auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -mfpu=neon -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o neon.o neon.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [neon.o] Error 1
neon disabled.
ipc_sysv auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o ipc.o ipc.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [ipc.o] Error 1
ipc_sysv disabled.
ipc_posix auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o ipc.o ipc.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [ipc.o] Error 1
ipc_posix disabled.
libtiff auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o libtiff.o libtiff.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [libtiff.o] Error 1
libtiff disabled.
libmng auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o libmng.o libmng.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [libmng.o] Error 1
libmng disabled.
DB2 auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o db2.o db2.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [db2.o] Error 1
DB2 disabled.
InterBase auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o ibase.o ibase.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [ibase.o] Error 1
InterBase disabled.
MySQL (thread-safe) auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o mysql.o ../mysql/mysql.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [mysql.o] Error 1
MySQL (thread-safe) disabled.
MySQL (thread-unsafe) auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o mysql.o mysql.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [mysql.o] Error 1
MySQL (thread-unsafe) disabled.
OCI auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o oci.o oci.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [oci.o] Error 1
OCI disabled.
ODBC auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o odbc.o odbc.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [odbc.o] Error 1
ODBC disabled.
iODBC auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o iodbc.o iodbc.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [iodbc.o] Error 1
iODBC disabled.
PostgreSQL auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o psql.o psql.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [psql.o] Error 1
PostgreSQL disabled.
SQLite2 auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o sqlite2.o sqlite2.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [sqlite2.o] Error 1
SQLite2 disabled.
unknown SQL driver: sqlite_symbian
unknown SQL driver: symsql
TDS auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o tds.o tds.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [tds.o] Error 1
TDS disabled.
NIS auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o nis.o nis.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [nis.o] Error 1
NIS disabled.
Cups auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o cups.o cups.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [cups.o] Error 1
Cups disabled.
D-Bus auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o dbus.o dbus.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [dbus.o] Error 1
D-Bus disabled.
Glib auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o glib.o glib.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [glib.o] Error 1
Glib disabled.
ICU auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o icu.o icu.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [icu.o] Error 1
ICU disabled.
PulseAudio auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o pulseaudio.o pulseaudio.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [pulseaudio.o] Error 1
PulseAudio disabled.
OpenGL ES 2.x auto-detection... ()
arm-fsl-linux-gnueabi-g++ -c -pipe -O2 -O2 -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -I../../../mkspecs/qws/linux-imx6-g++ -I. -I/tftpboot/rootfs/usr/include -I/tftpboot/rootfs/usr/include/arm-linux-gnueabi/ -o opengles2.o opengles2.cpp
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make: *** [opengles2.o] Error 1
OpenGL ES 2.x disabled.
The OpenGL ES 2.0 functionality test failed!
You might need to modify the include and library search paths by editing
QMAKE_INCDIR_OPENGL_ES2, QMAKE_LIBDIR_OPENGL_ES2 and QMAKE_LIBS_OPENGL_ES2 in
/home/vishva/qt/mkspecs/qws/linux-imx6-g++.
Is there any problem in the command i gave??
I tried configuring with the below settings and during make getting following error
./configure -arch arm -xplatform qws/linux-imx6-g++ -release -prefix /tftpboot/ltib/usr/local/Trolltech/Qt-4.7.2-mx5x-x11 -multimedia -phonon -phonon-backend -qt-gfx-linuxfb -qt-kbd-tty -little-endian -host-little-endian -fontconfig -sm -opengl es2
Error:
cc1plus: error: /tftpboot/rootfs/usr/include: Too many levels of symbolic links
cc1plus: error: /tftpboot/rootfs/usr/include/arm-linux-gnueabi/: Too many levels of symbolic links
make[1]: *** [.pch/release-shared/QtCore.gch/c++] Error 1
make[1]: Leaving directory `/home/vishva/qt/src/corelib'
make: *** [sub-corelib-make_default-ordered] Error 2