Hello all,
I have been working with programming the OTP bits and am able to build and boot the pitc_otp_mfg_mx28 program and have it burn the bits just fine. What I want to know, is if there is a command that the pitc_otp_mfg_mx28 can receive that can reboot the iMX to start using the information programmed in?
Essentially, I am programming the CRYPTO bits and want to load another program over USB, but it expects the CRYPTO keys to be in effect. Is there a command to reboot and make these CRYPTO keys take effect? I am using the MFG tool on Windows to do this. Alternatively, is there a place I can get the source code for pitc_otp_mfg_mx28 and build it in myself?
Thanks
已解决! 转到解答。
Hi Trevor
unfortunately there is no command to reboot.
Also sources pitc_otp_mfg_mx28 are not available for customers.
As alternative it may be suggested to use OBDS (it has fuse program example)
IMX_OBDS : On-Board Diagnostic Suit for the i.MX28.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Trevor
unfortunately there is no command to reboot.
Also sources pitc_otp_mfg_mx28 are not available for customers.
As alternative it may be suggested to use OBDS (it has fuse program example)
IMX_OBDS : On-Board Diagnostic Suit for the i.MX28.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------