Reboot iMX from pitc_otp_mfg_mx28

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Reboot iMX from pitc_otp_mfg_mx28

跳至解决方案
1,441 次查看
trevork
Contributor I

Hello all,

I have been working with programming the OTP bits and am able to build and boot the pitc_otp_mfg_mx28 program and have it burn the bits just fine.  What I want to know, is if there is a command that the pitc_otp_mfg_mx28 can receive that can reboot the iMX to start using the information programmed in?

Essentially, I am programming the CRYPTO bits and want to load another program over USB, but it expects the CRYPTO keys to be in effect.  Is there a command to reboot and make these CRYPTO keys take effect?  I am using the MFG tool on Windows to do this. Alternatively, is there a place I can get the source code for pitc_otp_mfg_mx28 and build it in myself?

Thanks

标签 (1)
0 项奖励
回复
1 解答
1,307 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Trevor

unfortunately there is no command to reboot.

Also sources pitc_otp_mfg_mx28 are not available for customers.

As alternative it may be suggested to use OBDS (it has fuse program example)

IMX_OBDS : On-Board Diagnostic Suit for the i.MX28.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,308 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Trevor

unfortunately there is no command to reboot.

Also sources pitc_otp_mfg_mx28 are not available for customers.

As alternative it may be suggested to use OBDS (it has fuse program example)

IMX_OBDS : On-Board Diagnostic Suit for the i.MX28.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,307 次查看
trevork
Contributor I

Thank you for letting me know.  I'll look in to the OBDS.

0 项奖励
回复