Hi,
I have been trying to do this for quite some time now,
I have a custom imx6Q board which has the 25 Address lines, Lower order 16 bit data bus , OE, WE and CS1 connected to an Altera FPGA.
My aim was to generate a ROM in the FPGA and read it from the Microprocessor.
I was successfully able to do it. I will explain the steps below in order to replicate the scenario.
Step 1: Build the Ltib with Sabre-AI_weimnor u-boot and Sabre-AI kernel.
Assert the following in the kernel configuration
CONFIG_MTD_ROM=y
and make sure,
CONFIG_MTD_PHYSMAP=y
Step 2: I have attached the board-mx6q_sabreauto.c and board-mx6q_sabreauto.h files so that you may find the register settings and the iomux settings there.
In board-mx6q_sabreauto.h:
static iomux_v3_cfg_t mx6q_weimnor_pads[] __initdata = {
/* Parallel NOR */
MX6Q_PAD_EIM_OE__WEIM_WEIM_OE,
MX6Q_PAD_EIM_RW__WEIM_WEIM_RW,
MX6Q_PAD_EIM_CS1__WEIM_WEIM_CS_1,
/*Control NOR reset using gpio mode*/
/* Parallel Nor Data Bus */
MX6Q_PAD_CSI0_DATA_EN__WEIM_WEIM_D_0,
MX6Q_PAD_CSI0_VSYNC__WEIM_WEIM_D_1,
MX6Q_PAD_CSI0_DAT4__WEIM_WEIM_D_2,
MX6Q_PAD_CSI0_DAT5__WEIM_WEIM_D_3,
MX6Q_PAD_CSI0_DAT6__WEIM_WEIM_D_4,
MX6Q_PAD_CSI0_DAT7__WEIM_WEIM_D_5,
MX6Q_PAD_CSI0_DAT8__WEIM_WEIM_D_6,
MX6Q_PAD_CSI0_DAT9__WEIM_WEIM_D_7,
MX6Q_PAD_CSI0_DAT12__WEIM_WEIM_D_8,
MX6Q_PAD_CSI0_DAT13__WEIM_WEIM_D_9,
MX6Q_PAD_CSI0_DAT14__WEIM_WEIM_D_10,
MX6Q_PAD_CSI0_DAT15__WEIM_WEIM_D_11,
MX6Q_PAD_CSI0_DAT16__WEIM_WEIM_D_12,
MX6Q_PAD_CSI0_DAT17__WEIM_WEIM_D_13,
MX6Q_PAD_CSI0_DAT18__WEIM_WEIM_D_14,
MX6Q_PAD_CSI0_DAT19__WEIM_WEIM_D_15,
/* Parallel Nor 25 bit Address Bus */
MX6Q_PAD_EIM_A25__WEIM_WEIM_A_25,
MX6Q_PAD_EIM_A24__WEIM_WEIM_A_24,
MX6Q_PAD_EIM_A23__WEIM_WEIM_A_23,
MX6Q_PAD_EIM_A22__WEIM_WEIM_A_22,
MX6Q_PAD_EIM_A21__WEIM_WEIM_A_21,
MX6Q_PAD_EIM_A20__WEIM_WEIM_A_20,
MX6Q_PAD_EIM_A19__WEIM_WEIM_A_19,
MX6Q_PAD_EIM_A18__WEIM_WEIM_A_18,
MX6Q_PAD_EIM_A17__WEIM_WEIM_A_17,
MX6Q_PAD_EIM_A16__WEIM_WEIM_A_16,
MX6Q_PAD_EIM_DA15__WEIM_WEIM_DA_A_15,
MX6Q_PAD_EIM_DA14__WEIM_WEIM_DA_A_14,
MX6Q_PAD_EIM_DA13__WEIM_WEIM_DA_A_13,
MX6Q_PAD_EIM_DA12__WEIM_WEIM_DA_A_12,
MX6Q_PAD_EIM_DA11__WEIM_WEIM_DA_A_11,
MX6Q_PAD_EIM_DA10__WEIM_WEIM_DA_A_10,
MX6Q_PAD_EIM_DA9__WEIM_WEIM_DA_A_9,
MX6Q_PAD_EIM_DA8__WEIM_WEIM_DA_A_8,
MX6Q_PAD_EIM_DA7__WEIM_WEIM_DA_A_7,
MX6Q_PAD_EIM_DA6__WEIM_WEIM_DA_A_6,
MX6Q_PAD_EIM_DA5__WEIM_WEIM_DA_A_5,
MX6Q_PAD_EIM_DA4__WEIM_WEIM_DA_A_4,
MX6Q_PAD_EIM_DA3__WEIM_WEIM_DA_A_3,
MX6Q_PAD_EIM_DA2__WEIM_WEIM_DA_A_2,
MX6Q_PAD_EIM_DA1__WEIM_WEIM_DA_A_1,
MX6Q_PAD_EIM_DA0__WEIM_WEIM_DA_A_0,
};
In board-mx6q_sabreauto.c :
static void mx6q_setup_weimcs(void)
{
void __iomem *nor_reg = MX6_IO_ADDRESS(WEIM_BASE_ADDR);
void __iomem *ccm_reg = MX6_IO_ADDRESS(CCM_BASE_ADDR);
////////////////////*******************************///////////////////////
void __iomem *mx6q_iomuxc_reg = MX6_IO_ADDRESS(MX6Q_IOMUXC_BASE_ADDR);
////////////////////*******************************///////////////////////
unsigned int reg;
struct clk *clk;
u32 rate;
/* CLKCTL_CCGR6: Set emi_slow_clock to be on in all modes */
reg = readl(ccm_reg + 0x80);
reg |= 0x00000C00;
writel(reg, ccm_reg + 0x80);
clk = clk_get(NULL, "emi_slow_clk");
if (IS_ERR(clk))
printk(KERN_ERR "emi_slow_clk not found\n");
rate = clk_get_rate(clk);
if (rate != 132000000)
printk(KERN_ERR "Warning: emi_slow_clk not set to 132 MHz!"
" WEIM NOR timing may be incorrect!\n");
/* For EIM chip select configuration
* map the 128MB to chip select 2 which
* is connected to the FPGA.
*
* IOMUXC_GPR1:
* ADDRS3[10] = 00;
* ACT_CS3 = 0;
* ADDRS2[10] = 00;
* ACT_CS2 = 0;
* ADDRS1[10] = 10;
* ACT_CS1 = 1;
* ADDRS1[10] = 00;
* ACT_CS1 = 0;
*/
writel(0x48400028, mx6q_iomuxc_reg + 0x00000004);
writel(0x00610081, nor_reg + 0x00000018);
writel(0x00000001, nor_reg + 0x0000001C);
writel(0x1c020000, nor_reg + 0x00000020);
writel(0x00000000, nor_reg + 0x00000024);
writel(0x0804a240, nor_reg + 0x00000028);
writel(0x00000000, nor_reg + 0x0000002C);
}
static struct physmap_flash_data nor_flash_data = {
.probe_type = "map_rom",
.width = 2,
.parts = mxc_nor_partitions,
.nr_parts = ARRAY_SIZE(mxc_nor_partitions),
};
Step 3: I modified the boot parameters to initialize the weim-nor interface. I have attached the sabreauto_weimor.h file which contains the boot parameters.
In sabreauto_weimnor.h :
bootargs_base=setenv bootargs console=ttymxc0,115200
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp
nfsroot=${serverip}:${nfsroot},v3,tcp
bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel};
bootm
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait
weim-nor video=mxcfb0:dev=ldb,640x480M@60,if=RGB666 ldb=sep0
bootcmd_mmc1=run bootargs_base bootargs_mmc; mmc dev 2; mmc read ${loadaddr}
0x800 0x2000; bootm
bootcmd=run bootcmd_mmc
bootargs_nor=setenv bootargs ${bootargs} root=/dev/mtdblock3 rw
rootfstype=jffs2 ip=none weim-nor
bootcmd_mmc=run bootargs_base bootargs_mmc; cp.l 0x8080000 ${loadaddr}
0x400000; bootm
Step 4: I then booted my board with the kernel and rootfs.
Step 5: I configured the FPGA to include a ROM mapped to the EIM bus of the processor as specified above. I used the memtool utility to read the memory from the FPGA.
$cd /
$cd unit_tests
Usage:
Read:
/unit_tests $ ./memtool <-8, -16, -32> <Physical address> <count>
You can now observe the data read from the FPGA.
I am now trying to write data to the FPGA. I will add it to this document once it is complete.
regards,
Nishad
Original Attachment has been moved to: board-mx6q_sabreauto.h.zip
Original Attachment has been moved to: board-mx6q_sabreauto.c.zip
Original Attachment has been moved to: mx6q_sabreauto_weimnor.h.zip
Thank you for your time.
It is very good for me. i also to be try emi from fpga.