imx6 uart 带宽问题

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6 uart 带宽问题

跳至解决方案
2,076 次查看
zengzhaoping
Contributor II

imx6q uart带宽问题:

现在项目准备采样uart传输蓝牙音频数据,但是对imx6 uart的带宽有点疑问,

i.MX 6Dual/6Quad Linux Reference Manual.pdf中的描述是

• Standard Linux baud rates up to 4 Mbps

1、波特率的单位是bps?

2、内核driver(serial_core.c) 支持的最大波特率是921600;如果波特率为 921600转化为bps是多少?

3、how to up to 4Mbps?

标签 (3)
0 项奖励
回复
1 解答
1,753 次查看
jimmychan
NXP TechSupport
NXP TechSupport

1.  bps = baud per second x the number of bit per baud. Now, bit per baud is 1 bit because only 0 or 1. So, Baud rate = Bit rate.

2. 921600 bps.

3. The fastest module clock is 66.5MHz. So the UART max. baud rate is 4.15Mbit/s. (for details, please read the i.MX6Q RM Chapter 64.4.2.2 Maximum Baud Rate).

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,754 次查看
jimmychan
NXP TechSupport
NXP TechSupport

1.  bps = baud per second x the number of bit per baud. Now, bit per baud is 1 bit because only 0 or 1. So, Baud rate = Bit rate.

2. 921600 bps.

3. The fastest module clock is 66.5MHz. So the UART max. baud rate is 4.15Mbit/s. (for details, please read the i.MX6Q RM Chapter 64.4.2.2 Maximum Baud Rate).

0 项奖励
回复