Reading Keypad Data Register crashes i.MX 7 SoC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reading Keypad Data Register crashes i.MX 7 SoC

1,212 Views
falstaff
Senior Contributor I

Hello,

Our customer discovered a kernel freeze when trying to initialize the Keypad driver in Linux. Looking a bit closer in why it exactly freezes we could pinpoint a single register read during the drivers initialization: In imx_keypad_config the driver reads the Keypad Data Register (KPDR) on which line the system freezes.

static void imx_keypad_config(struct imx_keypad *keypad)
{
         unsigned short reg_val;

         /*
          * Include enabled rows in interrupt generation (KPCR[7:0])
          * Configure keypad columns as open-drain (KPCR[15:8])
          */
         reg_val = readw(keypad->mmio_base + KPCR);
         reg_val |= keypad->rows_en_mask & 0xff; /* rows */
         reg_val |= (keypad->cols_en_mask & 0xff) << 8; /* cols */
         writew(reg_val, keypad->mmio_base + KPCR);

         /* Write 0's to KPDR[15:8] (Colums) */
         reg_val = readw(keypad->mmio_base + KPDR);<FREEZE>
         reg_val &= 0x00ff;
         writew(reg_val, keypad->mmio_base + KPDR);

We can also verify that with a simple read using U-Boot.. Other register in the same block seem to work fine:

=> md.w 0x30320004 1
30320004: 0000 ..
=> md.w 0x30320002 1
30320002: 0002 ..
=> md.w 0x30320006 1
30320006:<FREEZE>

As far as I understand there should be no limitations on when this register is readable. It is only byte or half-word addressable, and md.w is addressing it using a half-word read, so this should be a valid register access.

This is reproducible on our Colibri iMX7 modules as well as on a NXP MCIMX7SABRE Rev. C (mask 2N09P). I did not found a related errata.

Best regards,

Stefan

Labels (2)
0 Kudos
Reply
3 Replies

933 Views
igorpadykov
NXP Employee
NXP Employee

Hi Stefan

usually hanging occurs due to clock absence, so one can check

if kpp clock is gated, please check CCM_CCGR170 Table 5-19. CCGR Mapping Table 

i.MX7D Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Additionally RDC module can impose access restrictions.

It may be useful to check read/write with jtag.

In linux one can look at kpp imx6sl-evk.dts

linux-2.6-imx.git - Freescale i.MX Linux Tree 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

933 Views
falstaff
Senior Contributor I

Hm, I first thought of clocks, too, but checked the gate mentioned in Chapter 5, Table 5-12:

ModuleModule Clock (instance.clock)Clock RootModule Clock Gating
Enable (CCGR)
KPPkpp.ipg_clk_sIPG_CLK_ROOTclk_enable_kpp (CCGR120)

So after checking CCGR120, I was convinced that clocking is fine, especially since the rest of the registers seemed to work...

Anyway, now after enabling the correct gate, CCGR170, the register at offset 6 is readable too! I guess CCGR120 in the table above is an error in the reference manual....

Thanks

Best regards,

Stefan

933 Views
markruthenbeck
NXP Employee
NXP Employee

All,

Thank you for finding and pointing out the errors in the reference manual. I do want to point you to table 5-19 which is the CCGR Mapping Table, which shows CCM_CCGR_170 for the KPP module.

It appears the correct data is shown in table 5-19 and incorrect in table 5-12. I have made the corrections in our systems.

thanks again,

mark

0 Kudos
Reply