Re: Importing 1050-EVK files into Altium

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: Importing 1050-EVK files into Altium

575 Views
gredpath
Contributor III

Would it be possible to get an ascii export of the .brd file. This would be an extension .alg, Altium can then import this, but this file can only be created from a Allegro licensed PC.

Regards

George

0 Kudos
Reply
1 Reply

493 Views
Yuri
NXP Employee
NXP Employee

Hello,

   I've sent You the .alg file via e-maul.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply