RT1170的SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1170的SDRAM

843 Views
Zyj
Contributor I

RT1176支持多片选操作SDRAM吗?

Labels (1)
0 Kudos
Reply
3 Replies

545 Views
StephenYeh
Contributor III

Hi Jeremy

感谢您的回覆,

请问若是在RT1172上只接SDRAM (16 bit)也是可正常运行的对吗?其它pin 状态是否floating即可。

 

0 Kudos
Reply

706 Views
StephenYeh
Contributor III

Hi Jeremy

请问每个CS 可以支持的是64MB,若是4个CS就是64MB *4对吗?

0 Kudos
Reply

839 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
非常感谢使用NXP产品,很高兴为你提供技术支持!
1) RT1176支持多片选操作SDRAM吗?
-- 是的。
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply