Background:
CPU:MCIMX6S5EVM10AB
Board design reference: SPF-27516_C3(Sabre-SDB)
Questions:
1,Customer want to set BT_CFG1_1(EIM_DA1) as high. Is it OK?
The reference schematics is set as DNP.
2, Customer's eMMC BUS width is set as 4bit, but customer set BT_CFG[7:5]=010:
The above image is from SPF-27516_C3 reference schematics. Should the BT_CFG[6:5] value change to x1?
3, For the BT_CFG3 and BT_CFG4, can they be set as NC?
已解决! 转到解答。
Hi 王 剑翰
1. I am afraid not, because EIM_DA1 BOOT_CFG1[1]
selects SD/eMMC Power Cycle Enable
Table 8-15. USDHC Boot eFUSE Descriptions IMX6SDLRM
2. yes for 4-bit width BT_CFG[6:5] value change to x1
3. BT_CFG3 and BT_CFG4 can be set as NC
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------