Dear team,
My customer is facing the issue that ECSPI module of i.MX6Q cannot communicate with a external SPI device on their proto-board.
They use i.MX6Q ECSPI as slave and the external device is the master.
Because the external device is the only SPI device, they do not use SS.
The SS pin of i.MX6 is open.
The customer’s configuration is as below.
ECSPI5_CONREG = 0x0170_D101
ECSPI5_CONFREG = 0x0000_0001
ECSPI5_INTREG = 0x0000_0028
ECSPI5_DMAREG = 0x0000_0000
ECSPI5_STATREG = 0x0000_0003
Could you give me advice on the cause of this issue?
Thanks,
Miyamoto
已解决! 转到解答。
Hi Miyamoto
yes SS pin of i.MX6 should be connected to external device
even if the SPI is used for peer-to-peer communication.
Best regards
igor
Hi AVNET JAPAN FAE
SS should be used in slave mode as describes
sect.21.4.2 Slave Mode IMX6DQRM :
In this configuration, Chip Select (SS) becomes an input signal, and is used to control
data transfers through the Shift register, as well as to load/store the data FIFO.
Also below one can find slave mode usage examples
i.MX6 ESPI slave mode support patch based on rel_imx_3.0.35_4.1.0
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------