Question, i.MX28 LRADC bandgap reference calibration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX28 LRADC bandgap reference calibration

ソリューションへジャンプ
1,037件の閲覧回数
Aemj
Contributor IV

Hi team,

I would like to ask about the bandgap reference voltage calibration.

i.MX28 reference manual(MCIMX28RM Rev.2) says as below.(Table 38-1)

"But if the bandgap reference is calibrated using the fuses, then …"

Could you show me what the 'calibration with fuses' is?

And could you show me the procedure of the calibrate with fuses?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 解決策
840件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi AVNET JAPAN FAE

ADC 'calibration with fuses' is not supported

(not tested/no example codes).

Also bandgap voltage doesn't output to pad and

can't be monitored on pad, so it is difficult to calibrate bandgap voltage for i.MX28.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
841件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi AVNET JAPAN FAE

ADC 'calibration with fuses' is not supported

(not tested/no example codes).

Also bandgap voltage doesn't output to pad and

can't be monitored on pad, so it is difficult to calibrate bandgap voltage for i.MX28.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
840件の閲覧回数
Aemj
Contributor IV

Hi Chipexpert,

Can I understand as below?

The internal bandgap reference voltage is connected to LRADC channel-14 internally, but user cannot monitor it.

Then the bandgap reference voltage cannot be calibrated.

BR,

Miyamoto

0 件の賞賛
返信
840件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

yes this is correct.

Best regards

chip

0 件の賞賛
返信