Hi, All.
I want to use each assigned port of i.MX6 ENET_MDC(KEY_COL2) and CAN1_TXCAN(KEY_COL2) , Do not use steering circuit like Sabre B'd(I atached a file).
Please, Inform me way to that question.
Best Regards,
Inho Jeon
Solved! Go to Solution.
Hi Inho
steering circuit is needed due to pinmux restrictions,
refer to attached Release Notes Table 10. Supported features
Supports both CANs using the flexcan device tree but has a pin conflict with FEC.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Inho
steering circuit is needed due to pinmux restrictions,
refer to attached Release Notes Table 10. Supported features
Supports both CANs using the flexcan device tree but has a pin conflict with FEC.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, igor !
Thank you for your reply.
You mean i.MX6 Dual lite is not supported port another CAN port not conflicted Ethenert port, is that right?
I want to using 2 of CAN and 1 of Ethenet at the same time by without steering circuit of I.MX6DL SABRE B'd.
How can I to do?
Please, inform me that way.
Best regards,
Inho Jeon
Hi Inho
I am afraid this is not possible on Sabre board, but if you are developing
new board one can try to allocate pads for such purpose using Processor Expert
Best regards
igor