Question, MX13892 XTAL2 routing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, MX13892 XTAL2 routing

ソリューションへジャンプ
638件の閲覧回数
Aemj
Contributor IV

Dear team,

My customer found a miss routing of MC13892/XTAL2 which is used with i.MX51 on their custom board.

We received from i.MX community the solution that XTAL2 should be connected to VCOREDIG pin when it is unused.

And the customer wants to know the exact reason why XTAL2 should be connected to VCOREDIG.

Could you give me the answer?

Actually, the rework that the customer connects XTAL2 and VCOREDIG is impossible on their board due to its PCD layout. Do you have any other ideas for the workaround?

The customer thinks that they can pull down XTAL2 to GND, or connect XTAL2 to GND on their board.

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 解決策
558件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

"If not used, XTAL1 should be connected to ground and XTAL2 to VCOREDIG.

This is for the internal detector circuit thresholds, there is a circuit which detects

whether a crystal is present or not."

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
559件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

"If not used, XTAL1 should be connected to ground and XTAL2 to VCOREDIG.

This is for the internal detector circuit thresholds, there is a circuit which detects

whether a crystal is present or not."

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信