Query about the RTC of I.MX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Query about the RTC of I.MX6Q

489件の閲覧回数
lukegu
Contributor I

Hi Dear ,

         When System is power down , how should the I.MX6Q operate to save the time data ,  and how to operate with the MMPF0100F0AEP ? Could you kindly help me to give some document to describe this issue ? Thanks !

ラベル(1)
0 件の賞賛
返信
1 返信

382件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  In order to implement RTC You may use scheme, based on i.MX6 reference design,

and follow Development Guide recommendations :

If VDD_SNVS_IN is directly supplied by a coin cell, a schottky diode is required between

VDD_HIGH_IN and VDD_SNVS_IN. The cathode is connected to VDD_SNVS_IN.

  From the Datasheet, Table 9 (Stop Mode Current and Power Consumption), there is

SNVS Only mode, when VDD_SNVS_IN powered and all other supplies off, and SRTC

is running.

SABRE Board Reference Design|NXP 

http://cache.nxp.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

http://cache.nxp.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信