Problems playing back audio using Qt 5.4 with gst-fsl-plugins-3.0.11

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems playing back audio using Qt 5.4 with gst-fsl-plugins-3.0.11

1,104 Views
ralph__
Contributor IV

I have upgraded my Qt installation from 5.3.2 to 5.4.1 and I find that I can no longer play back audio.

I am using QMediaPlayer to play an mp3 file back. The only thing that has changed in my iMX6 file system is the Qt version. Gstreamer and everything else is the same (version 0.1). "gplay" works fine for playing back the mp3 file. I am using pulseaudio and the normal sgtl5000 audio output (not HDMI audio).

Does anyone know why I can no longer play back audio files in Qt with QMediaPlayer?

Here is the output for reference:

# /usr/local/prototypes/qt_multimedia_test /usr/sample0.mp3

argc 3 /usr/sample0.mp3

Device name:  "sysdefault:CARD=imxhdmisoc"

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

List size =  0

Device name:  "default:CARD=imxhdmisoc"

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

List size =  0

Device name:  "sysdefault:CARD=imx6dlcolorsour"

List size =  0

Device name:  "default:CARD=imx6dlcolorsour"

List size =  0

Device name:  "default"

imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!

imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

List size =  0

Device name:  "alsa_output.0.analog-stereo"

List size =  1

Codec found:  "audio/pcm"

Play  "/usr/sample0.mp3"

(gst-plugin-scanner:267): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion 'GST_IS_PAD_TEMPLATE (templ)' failed

(gst-plugin-scanner:267): GStreamer-WARNING **: Failed to load plugin '/usr/lib/imx-mm/audio-codec/lib_src_ppp_arm11_elinux.so': /usr/lib/imx-mm/audio-codec/lib_src_ppp_arm11_elinux.so: undefined symbol: src_up2_prefilter_proc

QMultimedia::AvailabilityStatus is 0

QObject::startTimer: Timers can only be used with threads started with QThread

Beep: 3.0.11

Core: MP3 decoder Wrapper  build on Dec 25 2013 23:51:27

  mime: audio/mpeg, mpegversion = (int)1

  file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm12_elinux.so.3

CODEC: BLN_MAD-MMCODECS_MP3D_ARM_02.13.00_CORTEX-A8  build on Dec  5 2012 09:45:19.

Labels (4)
0 Kudos
1 Reply

563 Views
joanxie
NXP TechSupport
NXP TechSupport

the issue only happens on the qt5.4.1? what bsp version you use?

0 Kudos