There was no special CTP benchmarking provided for the i.MX28 series processors. The only point for the performance estimation is that the i.MX28 family processors are based on the ARM926 core that typically executes a single instruction per core clock. So, with the core operating frequency of 400MHz, the rough performance estimation can be made as 400MTOPS.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------