Problem for FT5x06 touch contoller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem for FT5x06 touch contoller

418 次查看
VictorWang129
Contributor II

Hello all, 

I am using I.MX6 Dual core, Linux kernel 4.1.15 to porting FT5x06 touch controller.

I am facing the problem of the touch could not work.

I have typed the command below to make sure the input device is.

cat /proc/bus/input/devices

VictorWang129_0-1682060069013.png

And also, I have confirmed that the driver can get the correct X & Y Positions.

However, it is still not working. Is it the problem with Vendor ID and Product ID? 

Could anyone help me with this? Thank you! 

 

标记 (2)
0 项奖励
回复
1 回复

388 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well.
 
Are you using a Polytouch touchscreen?
 
Please provide me with the device tree and bootlogs for further debugging.
 
Is the controller detected on the i2c bus using the i2cdetect command?
 
Thanks & Regards,
Sanket Parekh
0 项奖励
回复