Problem for FT5x06 touch contoller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem for FT5x06 touch contoller

414 Views
VictorWang129
Contributor II

Hello all, 

I am using I.MX6 Dual core, Linux kernel 4.1.15 to porting FT5x06 touch controller.

I am facing the problem of the touch could not work.

I have typed the command below to make sure the input device is.

cat /proc/bus/input/devices

VictorWang129_0-1682060069013.png

And also, I have confirmed that the driver can get the correct X & Y Positions.

However, it is still not working. Is it the problem with Vendor ID and Product ID? 

Could anyone help me with this? Thank you! 

 

Tags (2)
0 Kudos
Reply
1 Reply

384 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well.
 
Are you using a Polytouch touchscreen?
 
Please provide me with the device tree and bootlogs for further debugging.
 
Is the controller detected on the i2c bus using the i2cdetect command?
 
Thanks & Regards,
Sanket Parekh
0 Kudos
Reply