I'd like to start U-Boot from NAND Flash (MT29F2G08ABAEAH4), but I'm not going well.
The setting of BOOT_CFG is as follows.
Is the setting incorrect?
Or is it due to the old version of kobs - ng?
The CPU is i.MX6S.
BOOT_MODE0:1
BOOT_MODE1:0
BT_CFG1_0:0
BT_CFG1_1:0
BT_CFG1_2:0
BT_CFG1_3:0
BT_CFG1_4:1
BT_CFG1_5:0
BT_CFG1_6:1
BT_CFG1_7:1
BT_CFG2_0:0
BT_CFG2_1:1
BT_CFG2_2:0
BT_CFG2_3:0
BT_CFG2_4:0
BT_CFG2_5:0
BT_CFG2_6:0
BT_CFG2_7:0
Hi SHUNTARO
for nand boot please check sect.8.5.2 NAND Flash i.MX6SDL Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf
For nand programming please use mfg tools and bsp documentation on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------