Pins assign issue of "Pins for i.MX Version 2.0"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pins assign issue of "Pins for i.MX Version 2.0"

Jump to solution
860 Views
thanhnhatle
Contributor II

Hi,

In the tool "Pins for i.MX Version 2.0" for MCIMX7DxxVM and MCIMX7SxxVM, the following pins are not matched with datasheet.

Ball Name: DRAM_CAS_B
        datasheet : pin AC14
        Tool: pin AD17


Ball Name: DRAM_DQM1
        datasheet: pin pin AD17
        Tool: pin AC14

Could you please confirm that this is just the tool issue, not the datasheet?
Thank you and wait for your feedback.

Labels (2)
0 Kudos
Reply
1 Solution
768 Views
Yuri
NXP Employee
NXP Employee

Hello

  The values in the Datasheet are correct.

The ticket  for Pins Tool correction has been already submitted.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
769 Views
Yuri
NXP Employee
NXP Employee

Hello

  The values in the Datasheet are correct.

The ticket  for Pins Tool correction has been already submitted.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply