Peer to peer connection using broadr reach

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Peer to peer connection using broadr reach

1,119 次查看
ajayvenkatakris
Contributor II

Hi,

   I have two imx6 sabre AI boards with each supporting a BroadR reach PHY card. I have a peer to peer connection in between the boards. I have set up an ip address for both the boards, but while trying to ping between the boards, it says that the network is unreachable. The same set up has worked for the Atheros ENET phy Card. How do I set up the peer to peer connection between the two boards using broadr reach. Both the boards are running linaro Ubuntu.

Thanks,

Ajay Venkatakrishnan

0 项奖励
回复
4 回复数

980 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ajay

please create service request to obtain additional patch

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

980 次查看
ajayvenkatakris
Contributor II

Hi,

    What is patch required for?

Thank you,

Ajay V

0 项奖励
回复

980 次查看
igorpadykov
NXP Employee
NXP Employee

one board should be flashed with master (#define BCM89810_MASTER)
image and the other as slave image. Patch provides necessary definitions.

~igor

0 项奖励
回复

980 次查看
ajayvenkatakris
Contributor II

Hi,

    I have created the service request. Kindly provide the required patches and kindly mention how I can apply these patches? Also can I apply these patches for Linaro(Ubuntu) or only for Yocto?

0 项奖励
回复