Pciexpress slave on imx6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pciexpress slave on imx6Q

791件の閲覧回数
Selea
Senior Contributor I

DEar Sir,

the PCiexpress peripheral on imx6,could be master or slave, but what i see is that the linux driver use it only as a master... Is it available also something to use it as a slave?

The basic idea is to cluster at least two imx6Q ...

Any other idea to do that?

Thanks

Omar

ラベル(6)
0 件の賞賛
返信
2 返答(返信)

638件の閲覧回数
Selea
Senior Contributor I

I read that two RC (master) on PCIe could be "connected" using a not trasparent PCIe switch.. Anybody used such solution? Or can confirm me that it could works?

Thanks

Omar

0 件の賞賛
返信

638件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Omar,

You would need to modify the driver to set it as slave.

0 件の賞賛
返信