DEar Sir,
the PCiexpress peripheral on imx6,could be master or slave, but what i see is that the linux driver use it only as a master... Is it available also something to use it as a slave?
The basic idea is to cluster at least two imx6Q ...
Any other idea to do that?
Thanks
Omar
I read that two RC (master) on PCIe could be "connected" using a not trasparent PCIe switch.. Anybody used such solution? Or can confirm me that it could works?
Thanks
Omar
Hello Omar,
You would need to modify the driver to set it as slave.