PF0100 Default configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF0100 Default configuration

795件の閲覧回数
houdenglv
Contributor I

PWRON signal is used to turn on PMIC. It can be configured to detect a level, or an edge using the PWRON_CFG
bit as below. What's the default configuration of PWRON_CFG? 0 or 1?

pastedImage_2.png

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

656件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Devin

default fuse state is unprogrammed, 0.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------