Dear chip experts,
According to the SPF-27392_C4.pdf schematics, I tried to replace VGEN5 supply with optional LDO.
This LDO meets the additional current requirement but I worry about the startup timing.
- Is there any timing restrictions for LDO startup like VGEN5 startup sequece?
- If yes, in order to meet the timing, is it OK to input VGEN5 to the LDO pin5(SHDN*) instead of SYS_4V2?
- Does this option circuit already comfirmed and it worked if R32(0 ohrm) mounted ?
Can anybody help me?
Thanks.
Solved! Go to Solution.
Hello !
You may use the Optional LDO solution to supply both VDDHIGH_IN and VDD_SNVS_IN
of the i.MX6. On the scheme only VDD_SNVS_IN is provided by the LDO, “the optional LDO U9
shown on this page could be reconfigured to supply both VDDHIGH_IN and VDD_SNVS_IN”.
In such case there are no power sequence violation, assuming VDDHIGH_IN and VDD_SNVS_IN
turned on first.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello !
You may use the Optional LDO solution to supply both VDDHIGH_IN and VDD_SNVS_IN
of the i.MX6. On the scheme only VDD_SNVS_IN is provided by the LDO, “the optional LDO U9
shown on this page could be reconfigured to supply both VDDHIGH_IN and VDD_SNVS_IN”.
In such case there are no power sequence violation, assuming VDDHIGH_IN and VDD_SNVS_IN
turned on first.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------