OpenCL SoftISP demo works wrong on IMX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenCL SoftISP demo works wrong on IMX8MP

1,518 Views
quercuspau
Contributor II

Hello,

I am testing OpenCL capabilities on IMX8MP, currently im using the 8MPLUSLPD4-EVK evaluation board with BSP 5.10.72.

Tipping in the terminal from a pre-builded image:

root@imx8mpevk:/opt/imx-gpu-sdk/OpenCL/SoftISP# ./OpenCL.SoftISP --Enable
Denoise status: true
CycleNum status: 1000
Initializing device(s)...
Get the Device info and select Device...
# of Devices Available = 2
# of Compute Units = 1
# compute units = 1
Getting device id...
Creating Command Queue...
Creating kernels...
Please wait for compiling and building kernels, about one minute...
Kernel execution time on GPU (kernel: badpixel): 42.384 ms
Kernel execution time on GPU (kernel: sigma): 2.2427440000000014 ms
Kernel execution time on GPU (kernel: awb): 3.391982999999992 ms
Kernel execution time on GPU (kernel: equalize1): 8.101874 ms
Kernel execution time on GPU (kernel: equalize2): 0.388461000000001 ms
Kernel execution time on GPU (kernel: equalize3): 5.340270000000002 ms
Kernel execution time on GPU (kernel: debayer): 31.358999999999998 ms
Kernel execution time on GPU (kernel: rgba2yuyv): 23.354 ms
Kernel execution time on GPU (kernel: bilateral): 3014.373 ms
Kernel execution time on GPU (kernel: yuyv2rgba): 34.562 ms
Saving images...
root@imx8mpevk:/opt/imx-gpu-sdk/OpenCL/SoftISP# ls
0-SourceImage.bmp 1-RemoveBadPixel.bmp 2-WhiteBalance.bmp 3-Equalization.bmp 4-RemoveNoise.bmp Content OpenCL.SoftISP
root@imx8mpevk:/opt/imx-gpu-sdk/OpenCL/SoftISP#

The current bmp files look wrong, starting from 2-WhiteBalance.bmp. The current attachments are not the original files due the forum attachment limitation, but allow to see the overall problem.

0-SourceImage.png2-WhiteBalance.png3-Equalization.png4-RemoveNoise.png1-RemoveBadPixel.png

Is this a problem of the OpenCL implementation of the system or it is related to the demo itself?

The final goal is being able to codec RAW images in RGB format to jpeg using OpenCL.

Best Regards

 

Labels (2)
0 Kudos
Reply
5 Replies

1,504 Views
joanxie
NXP TechSupport
NXP TechSupport

i.mx8mp has HW ISP, why do you need softISP?

0 Kudos
Reply

1,497 Views
quercuspau
Contributor II

I am testing OpenCL on IMX8MP and NXP SoftISP demo doesn't work OK so Im wondering if OpenCL is well supported or demo has bugs.

0 Kudos
Reply

1,486 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

1,481 Views
quercuspau
Contributor II

AFAIK, imx8mp doesn't support OpenVx.

BR

0 Kudos
Reply

1,477 Views
joanxie
NXP TechSupport
NXP TechSupport

•This hardware extension is available in the i.MX8MP NPU, which means that OpenVX hardware acceleration is performed on the NPU, not on the GPU

0 Kudos
Reply