Greetings,
Can someone point me in the direction where OV5640 and OV5642 cameras compatible with the SabreSD board connectors can be found?
Regards,
Mete
Hi Atilla,
There isn't any compatible camera. To use them plug and play you must have the OV5640 and OV5642 modules.
You can check their availability on Omnivision distributors.
Best regards,
Rogerio
Did I ask something irrelevant?
Mete
for irrelevant question, you'd better create a new thread for it.
Just the modules that are plug and play for the Sabresd board, where to obtain them from.
Cheers,
Mete
let me remind, if you need them to use on nxp mx6 board, the board needs ov5640 or ov5642 module, I'm not sure you can get them from Omnivision.
Hello Joan,
To be honest, I was just asking the modules that are ready to use for Sabresd board. Sabre has connectors for OV5640 and OV5642, which modules are plugged to these connectors? Are they manufactured by NXP specifically for sabre board or does NXP get them from a 3rd party? (I am not speaking about Omnivision's Image Sensors itself but the modules build around them) If 3rd party, can you tell which one?
Kind regards,
Mete
what do you need? driver or schematic?