OV5640 and OV5642 Camera Modules compatible with SabreSD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OV5640 and OV5642 Camera Modules compatible with SabreSD

2,152 Views
atillametetured
Contributor V

 Greetings,

Can someone point me in the direction where OV5640 and OV5642 cameras compatible with the SabreSD board connectors can be found?

Regards,

Mete

Labels (3)
0 Kudos
7 Replies

1,402 Views
rogerio_silva
NXP Employee
NXP Employee

Hi Atilla,

There isn't any compatible camera. To use them plug and play you must have the OV5640 and OV5642 modules.

You can check their availability on Omnivision distributors.

Best regards,

Rogerio 

0 Kudos

1,402 Views
atillametetured
Contributor V

Did I ask something irrelevant?

Mete

0 Kudos

1,402 Views
joanxie
NXP TechSupport
NXP TechSupport

for irrelevant question, you'd better create a new thread for it.

0 Kudos

1,402 Views
atillametetured
Contributor V

Just the modules that are plug and play for the Sabresd board, where to obtain them from.

Cheers,

Mete

0 Kudos

1,402 Views
joanxie
NXP TechSupport
NXP TechSupport

let me remind, if you need them to use on nxp mx6 board, the board needs ov5640 or ov5642 module, I'm not sure you can get them from Omnivision.

0 Kudos

1,402 Views
atillametetured
Contributor V

Hello Joan,

To be honest, I was just asking the modules that are ready to use for Sabresd board. Sabre has connectors for OV5640 and OV5642, which modules are plugged to these connectors? Are they manufactured by NXP specifically for sabre board or does NXP get them from a 3rd party? (I am not speaking about Omnivision's Image Sensors itself but the modules build around them)  If 3rd party, can you tell which one?

Kind regards,

Mete

0 Kudos

1,402 Views
joanxie
NXP TechSupport
NXP TechSupport

what do you need? driver or schematic?

0 Kudos