OV420 driver for i.MX535 QSB and linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OV420 driver for i.MX535 QSB and linux

1,690 Views
aksispd
Contributor II

​I'm fairly new to i.MX and trying to connect an OV420 A/D with CMOS sensor to the I.MX535 QSB, anyone has experience with driver development? the supplied OV3640 seems to be a good start, is this the right way to get going? modify the existing Driver or start from scratch. Also did anyone make the test pattern work? Thanks!

0 Kudos
Reply
6 Replies

1,323 Views
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the drvier souce code of mx53 in the bsp, I don't have ov420 data sheet, if you use tvin as input, I can send the tvin demo source code to you for reference.

0 Kudos
Reply

1,323 Views
aksispd
Contributor II

Can you please send the TVin demo? By any chance did you have the csi test mode working from the system dev guide 19th section.

0 Kudos
Reply

1,323 Views
joanxie
NXP TechSupport
NXP TechSupport

pls find the demo code, hope helpful for you.

1,323 Views
aksispd
Contributor II

I have one more question, per the documentation the i.MX53 QSB-R does not support camera, I guess this only means there is no connector installed. If you build a daughterboard it should all work fine. Is that right?

0 Kudos
Reply

1,323 Views
aksispd
Contributor II

I plan using the CSI0 and trying to see if the example snippets shown in the i.MX53 System Development Guide 19th section. 

0 Kudos
Reply

1,323 Views
joanxie
NXP TechSupport
NXP TechSupport

if you use linux os, you can refer to the enclosed file to get the driver of bsp for other camera.

0 Kudos
Reply