ODT settings

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ODT settings

675 次查看
tkl
Contributor II

I found another thing, although this is in the script aid tool, I think the topic is related. When changing System ODT setting in the SI Configuration to 120,

0x021b001c =0x02008032

should be changed to

0x021b001c =0x04008032

from what I understand from the DDR2 MR2 register definition. But it stays on the 60 Ohm setting. Is this on purpose or a bug?

0 项奖励
回复
1 回复

551 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Values of 120 Ohms and 60 Ohms are typically used.

About ODT setting of DDR3 DQS in i.MX6DQ. 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复