Bug in DDR Stess Tester v 2.8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug in DDR Stess Tester v 2.8

491 Views
tkl
Contributor II

Hi,

i am using the DDR Stress Tester to get calibration values for DDR3 RAM. I think I stumbled across a bug. Here is part of the messages from the tool:

BYTE 0:
        Start:           HC=0x00 ABS=0x00
        End:             HC=0x02 ABS=0x50
        Mean:            HC=0x01 ABS=0x28
        End-0.5*tCK:     HC=0x01 ABS=0x50
        Final:           HC=0x01 ABS=0x50
BYTE 1:
        Start:           HC=0x00 ABS=0x30
        End:             HC=0x02 ABS=0x58
        Mean:            HC=0x01 ABS=0x44
        End-0.5*tCK:     HC=0x01 ABS=0x58
        Final:           HC=0x01 ABS=0x58

DQS calibration MMDC0 MPDGCTRL0 = 0x41D80150, MPDGCTRL1 = 0x00000000

If I am not mistaken, shouldn't the last line be

DQS calibration MMDC0 MPDGCTRL0 = 0x41580150, MPDGCTRL1 = 0x00000000

0 Kudos
1 Reply

325 Views
Yuri
NXP Employee
NXP Employee

Hello,

  DG_EXT_UP (DG extend upper boundary) bit is set, meaning the upper
boundary is set according to the last passing comparison. This is more reliable

configuration.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos