Not able to update latest BSP L4.1.15 on my custom iMX6Q board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to update latest BSP L4.1.15 on my custom iMX6Q board

1,529件の閲覧回数
vatsal_p
Contributor I

I have custom board of iMX6q working fine with L3.14.28 , need to update kernel to BSP L4.1.15 but im facing issue with boot up.

its hangs after following:

Uncompressing Linux... done, booting the kernel.
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.1.15-1.0.0 (xxxxxxx-VirtualBox) (gcc version 4.7.2 (GCC) ) #40 SMP PREEMPT Thu Apr 27 18:01:35 IST 2017
[    0.000000] Machine model: XXXXX i.MX6 Quad Board
[    0.000000] bootconsole [earlycon0] enabled
[    0.000000] Reserved memory: created CMA memory pool at 0x1c000000, size 320 MiB
[    0.000000] Reserved memory: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] PERCPU: Embedded 9 pages/cpu @8bb17000 s15872 r0 d20992 u36864
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
[    0.000000] Kernel command line: maxcpus=4 console=ttymxc0,115200 caam noinitrd video=vfb:0 cma=320M earlyprintk root=/dev/mmcblk0p1 ext3 rw rootwait  fpga=1 3
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 184696K/524288K available (4720K kernel code, 200K rwdata, 752K rodata, 268K init, 484K bss, 11912K reserved, 327680K cma-reserved)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
[    0.000000]     vmalloc : 0xa0800000 - 0xff000000   (1512 MB)
[    0.000000]     lowmem  : 0x80000000 - 0xa0000000   ( 512 MB)
[    0.000000]       .text : 0x80008000 - 0x80560428   (5474 kB)
[    0.000000]       .init : 0x80561000 - 0x805a4000   ( 268 kB)
[    0.000000]       .data : 0x805a4000 - 0x805d60c0   ( 201 kB)
[    0.000000]        .bss : 0x805d9000 - 0x80652014   ( 485 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]     Additional per-CPU info printed with stalls.
[    0.000000]     RCU kthread priority: 1.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] L2C-310 erratum 769419 enabled
[    0.000000] L2C-310 enabling early BRESP for Cortex-A9
[    0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[    0.000000] L2C-310 ID prefetch enabled, offset 16 lines
[    0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[    0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB
[    0.000000] L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76070001

Hangs.....

Also NOTE: i use same kernel build and load it in SABRESD board and it work.

igorpadykov‌  Carlos_Musich 

Help me, i don't know much about debugging kernel

PS: i saw some post in which if i comment disable_anatop_clocks(); function in "linux_4.1.15/arch/arm/mach-imx/clk-imx6q.c"  it will pass and it goes further but it wont able to read partition table from SD card.

i think bcoz i disable that function is related to parent_clock. please help.

Thanks in advance.

ラベル(2)
0 件の賞賛
返信
6 返答(返信)

1,297件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

To edit uboot the following guide will be useful as reference:

https://community.nxp.com/docs/DOC-328200 

Regards,

Carlos

0 件の賞賛
返信

1,297件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vatsal

image built for Sabre board may not work on custom board, due

to layout/ddr configs differencies. Please run ddr test

https://community.freescale.com/docs/DOC-105652 

find new calibration coefficients and put them in uboot/..mx6sabresd/*.cfg file

http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2015.04_4.1.15_1.0.0_ga

rebuild from scratch image, do not use files from L3.14.28

use linux documentation

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.0.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,297件の閲覧回数
vatsal_p
Contributor I

Hi Igor,

Thank you for reply, but i updated my DDR values in my bootloader ( we have custom boot-loader ) but still facing same issue.

I tried U-boot in my board but nothing appears, if i use SPL configuration then it display

Trying to boot from MMC1

spl: mmc partition switch failed
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

I did following changes in U-boot:

1. Updated DDR values.

2. change IOMUX for UART and MMC in board/../mxsabresd.c

i dont understand why its not able to read partition table at all.

NOTE: In My board we have used only one data pin for MMC, will it affect ? i.e., we using 3 pins: SD3_CLK , SD3_CMD, SD3_DATA0.

0 件の賞賛
返信

1,297件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vatsal

it should work also with only one data pin for MMC, please check in dts file:

&usdhc {
bus-width = <1>;

Best regards
igor

0 件の賞賛
返信

1,297件の閲覧回数
vatsal_p
Contributor I

Hi igorpadykov,

if i bypass disable_anatop_clocks() by comment then it pass further and hangs at:

[    1.120655] sdhci: Secure Digital Host Controller Interface driver
[    1.126851] sdhci: Copyright(c) Pierre Ossman
[    1.131249] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.137873] /soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified
[    1.145048] sdhci-esdhc-imx 2198000.usdhc: could not get ultra high speed state, work on normal mode
[    1.154680] sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found
[    1.219316] mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
[    1.219443] mmc0: mmc_rescan_try_freq: trying to init card at 400000 Hz
[    1.238562] mxc_vpu 2040000.vpu_fsl: VPU initialized
[    1.259704] Galcore version 5.0.11.41671
[    1.289091] mmc0: host does not support reading read-only switch, assuming write-enable
[    1.308344] mmc0: new high speed SDHC card at address aaaa
[    1.314829] mmcblk0: mmc0:aaaa SS08G 7.40 GiB

-----hangs----- after 60 sec watch dog timer restart system.

i check on sabresd board, after mmcblk0: mmc0:aaaa SS08G 7.40 GiB it will check for partition table. but in my case its not able to read. and hangs.

i have attached config file. help me is if i miss out anything.

0 件の賞賛
返信

1,297件の閲覧回数
vatsal_p
Contributor I

Hi Igor,

yes bus-width = <1>;

my board does not have cd(card detect) and wp(write protect) [its NC-Not connected]

0 件の賞賛
返信