Hi,
I am working on iMX258. I want to drive high and low on UPLL_BYPCLK line. I
configured this line with ALT5 functionality (GPIO), Since there is no PAD
configuration register for this line my level change doesn't effect the environment.
How can I drive different level on the pin UPLL_BYPCLK (GPIO[16]).
Regards,
suzan
已解决! 转到解答。
According to the i.MX25RM Table 4-18, UPLL_BYPCLK is only DVS can be configured.
=======================
Hysteresis Enable—Disabled
Drive Strength—Nominal
Pull/Keep Enable—Disabled
Pull Up/Down Configuration—100 KΩ PU
Open Drain Enable—Disabled
Drive Voltage Select—CFG (3.3 V)
Pull/Keep Select—Keep
Slew Rate—FAST
=======================
By default, the DVS is 3.3V.
You can change the setting in (Offset 0x0434) (IOMUXC_SW_PAD_CTL_GRP_DVS_CRM)
Please check if you set it correct.
According to the i.MX25RM Table 4-18, UPLL_BYPCLK is only DVS can be configured.
=======================
Hysteresis Enable—Disabled
Drive Strength—Nominal
Pull/Keep Enable—Disabled
Pull Up/Down Configuration—100 KΩ PU
Open Drain Enable—Disabled
Drive Voltage Select—CFG (3.3 V)
Pull/Keep Select—Keep
Slew Rate—FAST
=======================
By default, the DVS is 3.3V.
You can change the setting in (Offset 0x0434) (IOMUXC_SW_PAD_CTL_GRP_DVS_CRM)
Please check if you set it correct.