Iam using IMX.6q,iam trying to build android 5 image for my IMX.6q board,i followed Android_User's_Guide.pdf(freescale),,,,,,while compiling it is showing following error,please help me to solve this........
including ./system/media/camera/tests/Android.mk ...
including ./system/netd/client/Android.mk ...
including ./system/netd/server/Android.mk ...
including ./system/security/keystore-engine/Android.mk ...
including ./system/security/keystore/Android.mk ...
including ./system/security/softkeymaster/Android.mk ...
including ./system/vold/Android.mk ...
including ./tools/external/fat32lib/Android.mk ...
No private recovery resources for TARGET_DEVICE sabreauto_6q
make -C kernel_imx -j4 uImage ARCH=arm CROSS_COMPILE=`pwd`/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi- LOADADDR=0x10008000
make[1]: Entering directory `/home/sunil/myandroid/kernel_imx'
CHK include/generated/uapi/linux/version.h
CC scripts/mod/empty.o
arm-eabi-gcc: error trying to exec 'cc1': execvp: No such file or directory
make[3]: *** [scripts/mod/empty.o] Error 1
make[3]: *** Waiting for unfinished jobs....
CC scripts/mod/devicetable-offsets.s
arm-eabi-gcc: error trying to exec 'cc1': execvp: No such file or directory
make[3]: *** [scripts/mod/devicetable-offsets.s] Error 1
make[2]: *** [scripts/mod] Error 2
make[1]: *** [scripts] Error 2
make[1]: *** Waiting for unfinished jobs....
make[1]: Leaving directory `/home/sunil/myandroid/kernel_imx'
make: *** [out/target/product/sabreauto_6q/kernel] Error 2
#### make failed to build some targets (37 seconds) ####
Hi,
The recovery resources is not an error but merely a warning that says that you don't have a "recovery/res" folder inside you board device folder:
Cross Reference: /build/core/Makefile
As jimmychan said, your error is the cc1 missing command. Please make sure to install all the required packages before building as explained in the release documentation.
Regards,
Gary
seems the error is "error trying to exec 'cc1': execvp: No such file or directory"