Need your Help for imx6d pci bus problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need your Help for imx6d pci bus problem

834件の閲覧回数
sunyd
Contributor I

the error message just below,but don't know how to resolve it ,tnank you very mach

pastedImage_1.png

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

760件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi synid

"imx6q-cpufreq.. error" may be related to board design: please check

that it has pmic, as i.MX6Q Sabre SD reference board, refer to sect.2.5.3 CPU

Frequency Scaling (CPUFREQ), sect.2.5.2 PMIC PF Regulator attached Linux

Manual. Try to use nxp linux from source.codeaurora repository

linux-imx - i.MX Linux kernel 

May be recommended to recheck board with Sabre schematic on

Schematics (1)
Design files, including hardware schematics, Gerbers, and OrCAD files.
SABRE Platform for Smart Devices | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

760件の閲覧回数
sunyd
Contributor I

left is not ok, right is ok  ,about pci, the problem may be not realted to imx6q-cpufreq?

pcierror.PNG

0 件の賞賛
返信

760件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

"not ok" does not show errors, it also shows "link up" .

You can try to experiment attaching other pcie cards or

changing pcie card from good to bad and compare.

Best regards
igor

0 件の賞賛
返信