Need your Help for imx6d pci bus problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need your Help for imx6d pci bus problem

1,963 次查看
sunyd
Contributor I

the error message just below,but don't know how to resolve it ,tnank you very mach

pastedImage_1.png

标签 (1)
0 项奖励
回复
3 回复数

1,887 次查看
igorpadykov
NXP Employee
NXP Employee

Hi synid

"imx6q-cpufreq.. error" may be related to board design: please check

that it has pmic, as i.MX6Q Sabre SD reference board, refer to sect.2.5.3 CPU

Frequency Scaling (CPUFREQ), sect.2.5.2 PMIC PF Regulator attached Linux

Manual. Try to use nxp linux from source.codeaurora repository

linux-imx - i.MX Linux kernel 

May be recommended to recheck board with Sabre schematic on

Schematics (1)
Design files, including hardware schematics, Gerbers, and OrCAD files.
SABRE Platform for Smart Devices | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,887 次查看
sunyd
Contributor I

left is not ok, right is ok  ,about pci, the problem may be not realted to imx6q-cpufreq?

pcierror.PNG

0 项奖励
回复

1,887 次查看
igorpadykov
NXP Employee
NXP Employee

"not ok" does not show errors, it also shows "link up" .

You can try to experiment attaching other pcie cards or

changing pcie card from good to bad and compare.

Best regards
igor

0 项奖励
回复