Need for GPIO Pins correlation on iMx6 Ultralite Board:
I am using the i.MX6 Ultralite board.
But, I don't know the correlation between GPIO / GPIOCHIP #s and the actual pin #s.
Such as these would be useful (to start) :
J1703 - D0,D1,D2,D3,D4,D5,D6,D7
J1706 - A0,A1,A2,A3,A4,A5
J1704 - D8,D9,D10,D11,D12,D13,D14,D15
Thanks - in advance.
Actually I have tried most ALL of the 160 Pins using the SysFs script below, on the Ultralite board.
But, I see No Results on the Output Pins.
echo 23 > /sys/class/gpio/export
echo out > /sys/class/gpio/gpio23/direction
echo 1 > /sys/class/gpio/gpio23/value
So, I have NOT seen any output on the Any Pins.
... Anybody have any suggestions ?
Actually,
I have correlated the Pins to GPIO #s.
But, I am having trouble compiling the code.
I can create a simple Layer project.
But, when I attempt to include external files, like gpio.h ,
I only get back compile errors:
#include <linux/gpio.h>
Log data follows:
| DEBUG: Executing shell function do_compile
| helloworld.c:9:24: fatal error: linux/gpio.h: No such file or directory
| #include <linux/gpio.h>
| ^
| compilation terminated.
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/johnc/yocto_3.14.38-6UL/build/tmp/work/cortexa7hf-vfp-neon-poky-linux-gnueabi/myHelloWorld/0.1-r0/temp/log.do_compile.14565)
Even direct path includes:
#include "/home/johnc/yocto_3.14.38-6UL/build/tmp/work/cortexa7hf-vfp-neon-poky-linux-gnueabi/linux-libc-headers/3.14-r0/linux-3.14/include/linux/gpio.h"
Log data follows:
| DEBUG: Executing shell function do_compile
| In file included from helloworld.c:11:0:
| /home/johnc/yocto_3.14.38-6UL/build/tmp/work/cortexa7hf-vfp-neon-poky-linux-gnueabi/linux-libc-headers/3.14-r0/linux-3.14/include/linux/bug.h:4:21: fatal error: asm/bug.h: No such file or directory
| #include <asm/bug.h>
| ^
| compilation terminated.
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/johnc/yocto_3.14.38-6UL/build/tmp/work/cortexa7hf-vfp-neon-poky-linux-gnueabi/myHelloWorld/0.1-r0/temp/log.do_compile.14225)
-> How am I supposed to Include Files/Headers and/or modify the Include Paths ?
Hi john
one can use by pad name: for example J1703 -D1 UART2_TXD
sect.4.1.1 Muxing Options p.182 i.MX6UL Reference Manual (rev.0 8/2015) :
GPIO1_20. Then use Chapter 27 General Purpose Input/Output (GPIO)
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor, John,
I am also working with the imx6ulevk and trying to use simple gpio at arduino expansion connectors.
In order not to modify the device tree, I would like to use gpio_1, gpio_2, gpio_3 and gpio_4.
They are already defined as gpios in the device tree:
pinctrl_tsc: tscgrp {
fsl,pins = <
MX6UL_PAD_GPIO1_IO01__GPIO1_IO01 0xb0
MX6UL_PAD_GPIO1_IO02__GPIO1_IO02 0xb0
MX6UL_PAD_GPIO1_IO03__GPIO1_IO03 0xb0
MX6UL_PAD_GPIO1_IO04__GPIO1_IO04 0xb0
>;
};
For instance, in the case of GPIO_1 I do the following:
R1718ON / R906OFF / R1115OFF
and
root@imx6ulevk:/sys/class/gpio# echo 1 > /sys/class/gpio/export
root@imx6ulevk:/sys/class/gpio# echo out > /sys/class/gpio/gpio1/direction
root@imx6ulevk:/sys/class/gpio# echo 1 > /sys/class/gpio/gpio1/value
First thing that I don't understand is why
cat /sys/class/gpio/gpio1/value equals 0 when I have set it to 1.
Regarding voltage levels:
root@imx6ulevk:/sys/class/gpio# echo 1 > /sys/class/gpio/gpio1/value -> around 700mV
root@imx6ulevk:/sys/class/gpio# echo 0 > /sys/class/gpio/gpio1/value -> around 100mV
can anybody give me some advice on how to go on?
Thanks in advance!
BR
I am having problems compiling.
- See below.