imx6sx mxsfb error with QT5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6sx mxsfb error with QT5

Jump to solution
815 Views
peterbärtsch
Contributor III

Hi

We have only 256M RAM on our board. When I start QML Application I get mxsfb 2220000.lcdif: Unable to allocate framebuffer memory

cma: CMA: reserved 96 MiB at 8a000000

Memory policy: Data cache writealloc

PERCPU: Embedded 8 pages/cpu @89db1000 s8320 r8192 d16256 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024

Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk3p2 rootwait rw

PID hash table entries: 1024 (order: 0, 4096 bytes)

Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)

Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)

Memory: 146900K/262144K available (7035K kernel code, 394K rwdata, 6144K rodata, 320K init, 429K bss, 115244K reserved, 0K highmem)

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0x90800000 - 0xff000000   (1768 MB)

    lowmem  : 0x80000000 - 0x90000000   ( 256 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .text : 0x80008000 - 0x80ce6e80   (13180 kB)

      .init : 0x80ce7000 - 0x80d37080   ( 321 kB)

      .data : 0x80d38000 - 0x80d9a980   ( 395 kB)

       .bss : 0x80d9a98c - 0x80e05dd8   ( 430 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

Preemptible hierarchical RCU implementation.

    RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1

I increase the CMA memory to 160M (on EVK) and than it works. But on our board I can configure only 96M otherwise I get kernel panic.

Is the GPU Memory on a fix address or why does it not work with less then 160M CMA memory?

Peter

Labels (2)
0 Kudos
Reply
1 Solution
619 Views
peterbärtsch
Contributor III

Hi

I solve it with  QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1

Peter

View solution in original post

0 Kudos
Reply
1 Reply
620 Views
peterbärtsch
Contributor III

Hi

I solve it with  QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1

Peter

0 Kudos
Reply