Hi All,
I am working on Ethernet with IMX8QM Custom platform.
Ethernet: TJA1101 AUTO-PHY
Board: IMX8QM Custom Platform
Got log,
[ 2.043859] fec 5b040000.ethernet: Adding to iommu group 1
[ 2.120525] fec 5b040000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[ 2.127330] fec 5b040000.ethernet: Using random MAC address: 8a:c9:99:3f:4f:24
[ 2.145291] mdio_bus 5b040000.ethernet-1: MDIO device at address 1 is missing.
[ 2.152853] fec 5b040000.ethernet eth0: registered PHC device 0
[ 2.166432] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 2.200606] igb: Intel(R) Gigabit Ethernet Network Driver
[ 39.454726] NXP TJA1101 5b040000.ethernet-1:00: attached PHY driver [NXP TJA1101] (mii_bus:phy_addr=5b040000.ethernet-1:00, irq=POLL)
And link is not detected,
root@root:~# ifconfig eth0
eth0 Link encap:Ethernet HWaddr 8A:C9:99:3F:4F:24
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root@root:~# ethtool eth0
Settings for eth0:
Supported ports: [ TP ]
Supported link modes: 100baseT1/Full
Supported pause frame use: Symmetric
Supports auto-negotiation: No
Supported FEC modes: Not reported
Advertised link modes: 100baseT1/Full
Advertised pause frame use: Symmetric
Advertised auto-negotiation: No
Advertised FEC modes: Not reported
Speed: 100Mb/s
Duplex: Full
Auto-negotiation: off
master-slave cfg: forced master
Port: Twisted Pair
PHYAD: 0
Transceiver: external
MDI-X: Unknown
Supports Wake-on: g
Wake-on: d
Link detected: no
SQI: 0/7
I unable to get the ethernet link is up once connect ethernet cable with board and this is my configuration,
&fec1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec1>;
phy-mode = "rmii";
phy-handle = <ðphy0>;
fsl,magic-packet;
/* nvmem-cells = <&fec_mac0>;
nvmem-cell-names = "mac-address"; */
status = "okay";
local-mac-address = [32 9f 6f 77 0c 66];
mdio {
#address-cells = <1>;
#size-cells = <0>;
ethphy0: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0>;
/delete-property/ at803x,eee-disabled;
/delete-property/at803x,vddio-1p8v;
/delete-property/phy-supply;
/* at803x,eee-disabled;
at803x,vddio-1p8v;*/
/*tja110x,refclk_in; */
};
ethphy1: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <1>;
at803x,eee-disabled;
at803x,vddio-1p8v;
};
};
};
pinctrl_fec1: fec1grp {
fsl,pins = <
IMX8QM_COMP_CTL_GPIO_1V8_3V3_ENET_ENETB_PAD 0x000014a0
IMX8QM_ENET0_MDC_CONN_ENET0_MDC 0x06000020
IMX8QM_ENET0_MDIO_CONN_ENET0_MDIO 0x06000020
IMX8QM_ENET0_RGMII_TX_CTL_CONN_ENET0_RGMII_TX_CTL 0x06000061
IMX8QM_ENET0_RGMII_TXC_CONN_ENET0_RCLK50M_IN 0xce000061
IMX8QM_ENET0_RGMII_TXD0_CONN_ENET0_RGMII_TXD0 0x06000061
IMX8QM_ENET0_RGMII_TXD1_CONN_ENET0_RGMII_TXD1 0x06000061
IMX8QM_ENET0_RGMII_RX_CTL_CONN_ENET0_RGMII_RX_CTL 0x06000061
IMX8QM_ENET0_RGMII_RXD0_CONN_ENET0_RGMII_RXD0 0x06000061
IMX8QM_ENET0_RGMII_RXD1_CONN_ENET0_RGMII_RXD1 0x06000061
IMX8QM_ENET0_RGMII_RXD2_CONN_ENET0_RMII_RX_ER 0x0d000061
>;
};
已解决! 转到解答。
Hi,
Please close this ticket.
It is a hardware issue.
Hello,
set your device as master like this:
#echo 1 > /sys/devices/platform/soc@0/30800000.bus/30be0000.ethernet/mdio_bus/30be0000.ethernet-1/30be0000.ethernet-1:00/configuration/master_cfg
Regards
Thank you @AlfTeleco ,
I already did, it is the hardware issue and resolve by the hardware engineer.
By the way, I am currently debugging an ethernet-phy problem.
We are also using the TJA1101B in a setup with two custom IMX8MP boards.
Both are configured as AUTO_OP using pin strapping.
Once they are at linux, one is set as master ( echo 1 > master_cfg ) and the other remains as slave.
I assing IP to the eth0 iface and I can ping perfectly.
The problem comes when I reset the slave-phy board, the system prompts this trace at boot:
#mdio_bus 30be0000.ethernet-1: MDIO device at address 0 is missing.
#fec 30be0000.ethernet eth0: Unable to connect to phy
It seems that as long as a link between phys exists, the slave will fail to be detected by the system at boot.
Any idea on this? Thanks in advance!
Hi @AlfTeleco ,
Defined mac address under uboot env. if problem still exists define mac address under linux dts
Hi Vinothkumar
one can check "PHYADDRESS" settings as in example on p.23 SPF-29420 MCIMX8QM-CPU
schematic MCIMX8QM-CPU MEK – Schematics
use below dts
Best regards
igor
Thank you @igorpadykov for the reply,
Currently TJA1101 AUTO-PHY connect with phy0 of the IMX8QM custom board.
I am doubt about clock,
ENET0_REFCLK_125M_25M I cannot use because it is DNP.
For phy Master, Which one I have to configure (CLOCK_IN or CLOCK_OUT) ENET0_RGMII_TXC ?
IMX8QM_ENET0_RGMII_TXC_CONN_ENET0_RCLK50M_IN
(or)
IMX8QM_ENET0_RGMII_TXC_CONN_ENET0_RCLK50M_OUT
Hi,
Please close this ticket.
It is a hardware issue.
I'm trying to integrate TJA1101 Phy with IMX8M Custom board as 2 -wire ethernet interface. I'm also not able to get the link up.
root@imx8mpevk:/opt/imx8-isp/bin# ethtool eth0
Settings for eth0:
Supported ports: [ TP ]
Supported link modes: 100baseT1/Full
Supported pause frame use: Symmetric
Supports auto-negotiation: No
Supported FEC modes: Not reported
Advertised link modes: 100baseT1/Full
Advertised pause frame use: Symmetric
Advertised auto-negotiation: No
Advertised FEC modes: Not reported
Speed: 100Mb/s
Duplex: Full
Auto-negotiation: off
master-slave cfg: forced slave
Port: Twisted Pair
PHYAD: 0
Transceiver: external
MDI-X: Unknown
Supports Wake-on: g
Wake-on: d
Link detected: no
SQI: 0/7
root@imx8mpevk:/opt/imx8-isp/bin#
&fec {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec>;
phy-mode = "rmii";
phy-handle = <ðphy1>;
fsl,magic-packet;
status = "okay";
phy-reset-gpios = <&gpio3 0 0>;
phy-reset-duration = <10>;
mdio {
#address-cells = <1>;
#size-cells = <0>;
ethphy1: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0>;
tja110x,refclk_in;
};
};
};
pinctrl_fec: fecgrp {
fsl,pins = <
MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC 0x3
MX8MP_IOMUXC_SAI1_RXD3__ENET1_MDIO 0x3
MX8MP_IOMUXC_SAI1_RXD4__ENET1_RGMII_RD0 0x91
MX8MP_IOMUXC_SAI1_RXD5__ENET1_RGMII_RD1 0x91
MX8MP_IOMUXC_SAI1_TXD7__ENET1_TX_ER 0x1f
MX8MP_IOMUXC_SAI1_TXD4__ENET1_RGMII_TX_CTL 0x1f
MX8MP_IOMUXC_SAI1_TXD0__ENET1_RGMII_TD0 0x1f
MX8MP_IOMUXC_SAI1_TXD1__ENET1_RGMII_TD1 0x1f
MX8MP_IOMUXC_SAI1_TXFS__ENET1_RGMII_RX_CTL 0x91
MX8MP_IOMUXC_SAI1_TXD6__ENET1_RX_ER 0x1f
MX8MP_IOMUXC_SAI1_MCLK__ENET1_TX_CLK 0x3
/* MX8MP_IOMUXC_SAI1_RXD6__ENET1_RGMII_RD2 0x91 */
/* MX8MP_IOMUXC_SAI1_RXD7__ENET1_RGMII_RD3 0x91 */
/* MX8MP_IOMUXC_SAI1_TXC__ENET1_RGMII_RXC 0x91 */
/* MX8MP_IOMUXC_SAI1_TXD2__ENET1_RGMII_TD2 0x1f */
/* MX8MP_IOMUXC_SAI1_TXD3__ENET1_RGMII_TD3 0x1f */
/* MX8MP_IOMUXC_SAI1_TXD5__ENET1_RGMII_TXC 0x1f */
/* MX8MP_IOMUXC_SAI1_RXD0__GPIO4_IO02 0x19 */
>;
};
Im able to set the static IPs in 2 identical boards and not able to ping.
Is there any application/utility for read/write the PHY registers.
Also we have provided an ESD and common mode filter . Could you please confirm if its the same case with yours?
Any help is appreciated.
Regards
Amal