NXP i.MX8QM TJA1101 AUTO-PHY link is not up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP i.MX8QM TJA1101 AUTO-PHY link is not up

Jump to solution
3,895 Views
vinothkumars
Senior Contributor IV

Hi All,

 

I am working on Ethernet with IMX8QM Custom platform. 

Ethernet: TJA1101 AUTO-PHY

Board: IMX8QM Custom Platform

 

Got log,

[ 2.043859] fec 5b040000.ethernet: Adding to iommu group 1
[ 2.120525] fec 5b040000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[ 2.127330] fec 5b040000.ethernet: Using random MAC address: 8a:c9:99:3f:4f:24
[ 2.145291] mdio_bus 5b040000.ethernet-1: MDIO device at address 1 is missing.
[ 2.152853] fec 5b040000.ethernet eth0: registered PHC device 0
[ 2.166432] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 2.200606] igb: Intel(R) Gigabit Ethernet Network Driver
[ 39.454726] NXP TJA1101 5b040000.ethernet-1:00: attached PHY driver [NXP TJA1101] (mii_bus:phy_addr=5b040000.ethernet-1:00, irq=POLL)

 

And link is not detected,

root@root:~# ifconfig eth0

eth0 Link encap:Ethernet HWaddr 8A:C9:99:3F:4F:24
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

 

root@root:~# ethtool eth0
Settings for eth0:
Supported ports: [ TP ]
Supported link modes: 100baseT1/Full
Supported pause frame use: Symmetric
Supports auto-negotiation: No
Supported FEC modes: Not reported
Advertised link modes: 100baseT1/Full
Advertised pause frame use: Symmetric
Advertised auto-negotiation: No
Advertised FEC modes: Not reported
Speed: 100Mb/s
Duplex: Full
Auto-negotiation: off
master-slave cfg: forced master
Port: Twisted Pair
PHYAD: 0
Transceiver: external
MDI-X: Unknown
Supports Wake-on: g
Wake-on: d
Link detected: no
SQI: 0/7

 

I unable to get the ethernet link is up once connect ethernet cable with board and this is my configuration,

&fec1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec1>;
phy-mode = "rmii";
phy-handle = <&ethphy0>;
fsl,magic-packet;
/* nvmem-cells = <&fec_mac0>;
nvmem-cell-names = "mac-address"; */
status = "okay";
local-mac-address = [32 9f 6f 77 0c 66];
mdio {
#address-cells = <1>;
#size-cells = <0>;
ethphy0: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0>;
/delete-property/ at803x,eee-disabled;
/delete-property/at803x,vddio-1p8v;
/delete-property/phy-supply;

/* at803x,eee-disabled;
at803x,vddio-1p8v;*/
/*tja110x,refclk_in; */
};

ethphy1: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <1>;
at803x,eee-disabled;
at803x,vddio-1p8v;
};
};
};

pinctrl_fec1: fec1grp {
fsl,pins = <
IMX8QM_COMP_CTL_GPIO_1V8_3V3_ENET_ENETB_PAD 0x000014a0
IMX8QM_ENET0_MDC_CONN_ENET0_MDC 0x06000020
IMX8QM_ENET0_MDIO_CONN_ENET0_MDIO 0x06000020
IMX8QM_ENET0_RGMII_TX_CTL_CONN_ENET0_RGMII_TX_CTL 0x06000061
IMX8QM_ENET0_RGMII_TXC_CONN_ENET0_RCLK50M_IN 0xce000061
IMX8QM_ENET0_RGMII_TXD0_CONN_ENET0_RGMII_TXD0 0x06000061
IMX8QM_ENET0_RGMII_TXD1_CONN_ENET0_RGMII_TXD1 0x06000061
IMX8QM_ENET0_RGMII_RX_CTL_CONN_ENET0_RGMII_RX_CTL 0x06000061
IMX8QM_ENET0_RGMII_RXD0_CONN_ENET0_RGMII_RXD0 0x06000061
IMX8QM_ENET0_RGMII_RXD1_CONN_ENET0_RGMII_RXD1 0x06000061
IMX8QM_ENET0_RGMII_RXD2_CONN_ENET0_RMII_RX_ER 0x0d000061
>;
};

 

 

 

Regards,
Vinothkumar Sekar
0 Kudos
1 Solution
3,801 Views
vinothkumars
Senior Contributor IV

Hi,

 

Please close this ticket.

 

It is a hardware issue. 

 

The problem with Diode introduces in the following lines CONN_ETH_TRX_P and CONN_ETH_TRX_N for protection purpose because of that link is not detected.
 
After removing those two diodes, link is detected and ethernet is working.
 
 
Regards,
Vinothkumar Sekar

View solution in original post

0 Kudos
8 Replies
3,766 Views
AlfTeleco
Contributor III

Hello, 

 

set your device as master like this: 

 

#echo 1 > /sys/devices/platform/soc@0/30800000.bus/30be0000.ethernet/mdio_bus/30be0000.ethernet-1/30be0000.ethernet-1:00/configuration/master_cfg

 

Regards

0 Kudos
3,763 Views
vinothkumars
Senior Contributor IV

Thank you @AlfTeleco ,

 

I already did, it is the hardware issue and resolve by the hardware engineer.

Regards,
Vinothkumar Sekar
0 Kudos
3,756 Views
AlfTeleco
Contributor III

By the way, I am currently debugging an ethernet-phy problem. 

We are also using the TJA1101B in a setup with two custom IMX8MP boards.

Both are configured as AUTO_OP using pin strapping. 

Once they are at linux, one is set as master ( echo 1 > master_cfg ) and the other remains as slave. 

I assing IP to the eth0 iface and I can ping perfectly. 

The problem comes when I reset the slave-phy board, the system prompts this trace at boot:

#mdio_bus 30be0000.ethernet-1: MDIO device at address 0 is missing.

#fec 30be0000.ethernet eth0: Unable to connect to phy

It seems that as long as a link between phys exists, the slave will fail to be detected by the system at boot. 

Any idea on this? Thanks in advance!

 

0 Kudos
3,749 Views
vinothkumars
Senior Contributor IV

Hi @AlfTeleco ,

 

Defined mac address under uboot env. if problem still exists define mac address under linux dts

Regards,
Vinothkumar Sekar
0 Kudos
3,888 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

one can check "PHYADDRESS" settings as in example on p.23 SPF-29420 MCIMX8QM-CPU

schematic  MCIMX8QM-CPU MEK – Schematics

use below dts

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-enet2...

 

Best regards
igor

0 Kudos
3,880 Views
vinothkumars
Senior Contributor IV

Thank you @igorpadykov for the reply,

 

Currently TJA1101 AUTO-PHY connect with phy0 of the IMX8QM custom board.

I am doubt about clock,

 

ENET0_REFCLK_125M_25M I cannot use because it is DNP.

 

vinothkumars_0-1637047249786.png

 

For phy Master, Which one I have to configure (CLOCK_IN or CLOCK_OUT) ENET0_RGMII_TXC ?

IMX8QM_ENET0_RGMII_TXC_CONN_ENET0_RCLK50M_IN  

(or)

IMX8QM_ENET0_RGMII_TXC_CONN_ENET0_RCLK50M_OUT

 

 

Regards,
Vinothkumar Sekar
0 Kudos
3,802 Views
vinothkumars
Senior Contributor IV

Hi,

 

Please close this ticket.

 

It is a hardware issue. 

 

The problem with Diode introduces in the following lines CONN_ETH_TRX_P and CONN_ETH_TRX_N for protection purpose because of that link is not detected.
 
After removing those two diodes, link is detected and ethernet is working.
 
 
Regards,
Vinothkumar Sekar
0 Kudos
2,546 Views
Amal_Antony3331
Contributor III

Hi @vinothkumars 

I'm trying to integrate TJA1101 Phy with IMX8M Custom board as 2 -wire ethernet interface. I'm also not able to get the link up.

root@imx8mpevk:/opt/imx8-isp/bin# ethtool eth0
Settings for eth0:
        Supported ports: [ TP ]
        Supported link modes:   100baseT1/Full
        Supported pause frame use: Symmetric
        Supports auto-negotiation: No
        Supported FEC modes: Not reported
        Advertised link modes:  100baseT1/Full
        Advertised pause frame use: Symmetric
        Advertised auto-negotiation: No
        Advertised FEC modes: Not reported
        Speed: 100Mb/s
        Duplex: Full
        Auto-negotiation: off
        master-slave cfg: forced slave
        Port: Twisted Pair
        PHYAD: 0
        Transceiver: external
        MDI-X: Unknown
        Supports Wake-on: g
        Wake-on: d
        Link detected: no
        SQI: 0/7
root@imx8mpevk:/opt/imx8-isp/bin#
&fec {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_fec>;
        phy-mode = "rmii";
        phy-handle = <&ethphy1>;
        fsl,magic-packet;
        status = "okay";
        phy-reset-gpios = <&gpio3 0 0>;
        phy-reset-duration = <10>;

        mdio {
                #address-cells = <1>;
                #size-cells = <0>;

                ethphy1: ethernet-phy@0 {
                        compatible = "ethernet-phy-ieee802.3-c22";
                        reg = <0>;
                        tja110x,refclk_in;
                };
        };
};

       pinctrl_fec: fecgrp {
                fsl,pins = <
                        MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC               0x3
                        MX8MP_IOMUXC_SAI1_RXD3__ENET1_MDIO              0x3
                        MX8MP_IOMUXC_SAI1_RXD4__ENET1_RGMII_RD0         0x91
                        MX8MP_IOMUXC_SAI1_RXD5__ENET1_RGMII_RD1         0x91
                        MX8MP_IOMUXC_SAI1_TXD7__ENET1_TX_ER             0x1f
                        MX8MP_IOMUXC_SAI1_TXD4__ENET1_RGMII_TX_CTL      0x1f
                        MX8MP_IOMUXC_SAI1_TXD0__ENET1_RGMII_TD0         0x1f
                        MX8MP_IOMUXC_SAI1_TXD1__ENET1_RGMII_TD1         0x1f
                        MX8MP_IOMUXC_SAI1_TXFS__ENET1_RGMII_RX_CTL      0x91
                        MX8MP_IOMUXC_SAI1_TXD6__ENET1_RX_ER             0x1f
                        MX8MP_IOMUXC_SAI1_MCLK__ENET1_TX_CLK            0x3
/*                      MX8MP_IOMUXC_SAI1_RXD6__ENET1_RGMII_RD2         0x91 */
/*                      MX8MP_IOMUXC_SAI1_RXD7__ENET1_RGMII_RD3         0x91 */
/*                      MX8MP_IOMUXC_SAI1_TXC__ENET1_RGMII_RXC          0x91 */
/*                      MX8MP_IOMUXC_SAI1_TXD2__ENET1_RGMII_TD2         0x1f */
/*                      MX8MP_IOMUXC_SAI1_TXD3__ENET1_RGMII_TD3         0x1f */
/*                      MX8MP_IOMUXC_SAI1_TXD5__ENET1_RGMII_TXC         0x1f */
/*                      MX8MP_IOMUXC_SAI1_RXD0__GPIO4_IO02              0x19 */
                >;
        };

Im able to set the static IPs in 2 identical boards and not able to ping.

Is there any application/utility for read/write the PHY registers.

Also we have provided an ESD  and common mode filter . Could you please confirm if its the same case with yours?

Amal_Antony3331_0-1669094749341.png

 

Amal_Antony3331_1-1669094788735.pngAmal_Antony3331_2-1669094838399.png

 

Any help is appreciated.

Regards

Amal

0 Kudos