Yocto hardknott 15.10.72-2.2.2 imx8m-lpddr4-evk build error using Ubuntu 18.04

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto hardknott 15.10.72-2.2.2 imx8m-lpddr4-evk build error using Ubuntu 18.04

1,902 次查看
ejmfrancisco
Contributor I

Hi everyone,

I am trying to build Yocto Hardknott 15.10.72-2.2.2 on imx8m-lpddr-evk board using Ubuntu 18.04 host machine. I followed the "i.MX_Yocto_Project_User's_Guide.pdf" documentation as is and did not change anything. However, after multiple attempts, I keep on receiver error with exit code 1.

Can anyone tell me what seems to be the problem?

2qUhUlN-F1eW0vW1A6V3X7iuDmfOhuPAsxVCZRz1VucqqwLZ5Fuk7POXZVL7-OI6o3TsXjLVza4PghOYYvBEpO7w06a_Pfjs1Le5zGzIEYH3bvR-EVgCN8CuroAk.png

I tried clearing everything (builds, caches, and etc.) to re-build a fresh image but then, same error occurs every time.

I use these lines of code as well for set-up:

$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest  -b imx-linux-hardknott -m imx-5.10.72-2.2.2.xml

$: MACHINE=imx8mp-lpddr4-evk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b build-xwayland

Everything works fine until the "bitbake imx-image-full" command.

Thanks.

0 项奖励
回复
2 回复数

1,867 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @ejmfrancisco 

Have you installed those host packages as required for Yocto Project build? 

Can you share the error log?

 

Best regards

Harvey

0 项奖励
回复

1,830 次查看
ejmfrancisco
Contributor I

This one is solved thanks.

0 项奖励
回复