Hello All,
I'm sorry for my poor English in advance.
My system is consist of Linux Kernel boot + UBI Root Filesystem in iMX28.
I'm using the NAND (K9F1G08U) and I downloaded kernel and UBI Root F/S into NAND with Mfgtools(v1.62)
It usually works OK.
But some NAND have 2 kinds of problem as below.
1. Kernel panic happen.
2. Booting Error happen.
/************ Here is writing into the NAND flash with Mfgtools like as below *****************/
flash_eraseall /dev/mtd0
flash_eraseall /dev/mtd1
flash_eraseall /dev/mtd2
kobs-ng init imx28_ivt_linux.sb
/usr/bin/ubiattach /dev/ubi_ctrl -m 1 -d 0
mknod class/ubi,ubi0,/dev/ubi0
/usr/bin/ubimkvol /dev/ubi0 -n 0 -N rootfs0 -m
mkdir -p /mnt/ubi0; mount -t ubifs ubi0_0 /mnt/ubi0
tar -jmxv -C /mnt/ubi0 rootfs.tar.bz2
umount /mnt/ubi0
/usr/bin/ubiattach /dev/ubi_ctrl -m 2
mknod class/ubi,ubi1,/dev/ubi1
/usr/bin/ubimkvol /dev/ubi1 -n 0 -N data -m
mkdir -p /mnt/ubi1; mount -t ubifs ubi1_0 /mnt/ubi
cp -f usbdisk.img /mnt/ubi1/.
umount /mnt/ubi1
/****************************************************************/
1. Kernel Panic
/*******************************************************************************************/
:
UBIFS error (pid 1): ubifs_get_sb: cannot open "ubi0:rootfs1", error -19
VFS: Cannot open root device "ubi0:rootfs1" or unknown-block(0,0)
Please append a correct "root=" boot option; here are the available partitions:
1f00 20480 mtdblock0 (driver?)
1f01 94208 mtdblock1 (driver?)
1f02 16384 mtdblock2 (driver?)
fe00 89528 ubiblka (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
Backtrace:
[<c00324a8>] (dump_backtrace+0x0/0x114) from [<c03ca9f4>] (dump_stack+0x18/0x1c)
r7:c0029a24 r6:00008000 r5:c3048000 r4:c0740bb8
[<c03ca9dc>] (dump_stack+0x0/0x1c) from [<c03caa70>] (panic+0x78/0xf4)
[<c03ca9f8>] (panic+0x0/0xf4) from [<c000902c>] (mount_block_root+0x1d8/0x218)
r3:00000000 r2:00000001 r1:c3c23f78 r0:c047e0a5
[<c0008e54>] (mount_block_root+0x0/0x218) from [<c00091fc>] (prepare_namespace+0x94/0x1c4)
[<c0009168>] (prepare_namespace+0x0/0x1c4) from [<c00084f8>] (kernel_init+0x128/0x170)
r5:c00280c8 r4:c073fd00
[<c00083d0>] (kernel_init+0x0/0x170) from [<c004e570>] (do_exit+0x0/0x6dc)
r5:c00083d0 r4:00000000
/*******************************************************************************************/
I attached this kernel panic log( NandWritingUsingMfgtools_1.txt, Kernel_panic.txt)(nand_problem.zip)
NandWritingUsingMfgtools_1.txt : This is log when writing Kernel + UBI F/S in NAND using Mfgtools
Kernel_panic.txt : This is Kernel panic log.
2. BOOTING ERROR
/*******************************************************************************************/
HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFLC
PowerPrep start initialize power...
Configured for 5v only power source. Battery powered operation disabled
LLLCFeb 7 201416:51:56
FRAC 0x92925552
memory type is DDR2
Wait for ddr ready 1power 0x00820710
Frac 0x92925552
start change cpu freq
hbus 0x00000003
cpu 0x00010001
LLLLLLLFLCL0x8050100b
/*******************************************************************************************/
I attached this kernel panic log( NandWritingUsingMfgtools_2.txt, Booting_Error.txt)(nand_problem.zip)
NandWritingUsingMfgtools_2.txt : This is log when writing Kernel + UBI F/S in NAND using Mfgtools
Booting_Error.txt : This is Booting Error log.
Please help and give me any advices for this problems.
Thanks.
Original Attachment has been moved to: nand_problem.zip
Hi hongyup
from logs seems errors are no caused by NAND, but
poor power board design or DDR errors
You shoild modify power_prep sources (change brown-out levels)
to avoid 2. BOOTING ERROR. You can run with jtag to find
where exception occurs.
For NAND one can recheck below
Adding Support For a New NAND with i.MX28–NAND Analysis
Also it is highly recommended to check DDR with below tests
https://community.freescale.com/message/321913#321913
https://community.freescale.com/docs/DOC-1455
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your help.
I modified the brown-out levels in power_prep.c and DDR seting in init-mx28.c according to your recommend.
But I have still problems(2. BOOTING ERROR).
I downloaded small size file(imx28_ivt_uboot.sb, 142KB). It is OK.
//////////////////////////////////////////////////////////////////////////////////////////////////////
0x80501003
PowerPrep start initialize power...
Configured for 5v only power source. Battery powered operation disabled.
Feb 7 201416:51:56
FRAC 0x92925552
memory type is DDR2
Wait for ddr ready 1power 0x00820710
Frac 0x92925552
start change cpu freq
hbus 0x00000003
cpu 0x00010001
U-Boot 2009.08 (Jan 16 2014 - 18:01:24)
Freescale i.MX28 family
CPU: 454 MHz
BUS: 151 MHz
EMI: 205 MHz
GPMI: 24 MHz
DRAM: 128 MB
MMC: IMX_SSP_MMC: 0, IMX_SSP_MMC: 1
MMC0: No card detected!
MMC init failed
In: serial
Out: serial
Err: serial
Net: got MAC address from IIM: 00:04:00:00:00:00
FEC0
MX28 U-Boot >
//////////////////////////////////////////////////////////////////////////////////////////////////////////
Error Kernel boot(imx28_ivt_linux.sb, 2.5MB or 4.1MB).
I use bootles-5V-only and patched with L2.6.35_10.12_SDK_5V_SUPPLY_PATCH.tar.gz
Actuall I don't know what I change the brown-out levels?
Could you let me know more detail?
Thanks.
Hi hongyup
brownout is described in Chapter 11 i.MX28 RM.
You can know where exception occurs adding printfs to power_prep code
or running it with jtag.
For "Error Kernel boot" one can replace NAND chip
(may be they are weared out) or look at link below
Adding Support For a New NAND with i.MX28–NAND Analysis
Best regards
chip
Hi Chip
Thanks for your help.
Now I'm test with the NAND many things. But it have still problem.
Most of NAND works well. But it hapen some NAND.
And I move the problem NAND to another linux platform(mini2440 Board + uboot + linux) then It works.
Anyway, One of test is as below.
========================================
on Windows PC
>sb_loader -f imx28_ivt_linux.sb
...............................................................................Done.
waiting for Device Removal for 10seconds...
Device Removal event
========================================
It works.
Here is log when run sb_loader
======================================================================
HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFLC
hylim 0 _start : HW_RTC_PERSISTENT1_RD = [0x00000000]
.
PowerPrep start initialize power...
...
hylim 0 PowerPrep_ConfigurePowerSource : HW_RTC_PERSISTENT1_RD = [0x00000000]
hylim >> Configured for 5v only power source. Battery powered operation disabled.
..........
hylim 0-2 PowerPrep_ConfigurePowerSource : HW_RTC_PERSISTENT1_RD = [0x00000800]
hylim 1 PowerPrep_ConfigurePowerSource : HW_RTC_PERSISTENT1_RD = [0x00000800]
..LLLCMay 28 201416:16:17
FRAC 0x92925552
memory type is W9751G6JB DDR2
Wait for ddr ready 1power 0x00820710
Frac 0x92925552
start change cpu freq
hbus 0x00000003
cpu 0x00010001
LLLLLLLFLCLLJUncompressing Linux... done, booting the kernel.
Linux version 2.6.35.3-670-g914558e (hylim@hylim-virtual-machine) (gcc version 4.4.4 (4.4.4_09.06.2010) ) #1024 PREEMPT Tue May 13 12:08:09 KST 2014
============================================================================
But next is Nand booting error log
============================================================================
0x80501003
HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFLC
hylim 0 _start : HW_RTC_PERSISTENT1_RD = [0x00000002]
.
PowerPrep start initialize power...
...
hylim 0 PowerPrep_ConfigurePowerSource : HW_RTC_PERSISTENT1_RD = [0x00000002]
hylim >> Configured for 5v only power source. Battery powered operation disabled.
..........
hylim 0-2 PowerPrep_ConfigurePowerSource : HW_RTC_PERSISTENT1_RD = [0x00000802]
hylim 1 PowerPrep_ConfigurePowerSource : HW_RTC_PERSISTENT1_RD = [0x00000802]
..LLLCMay 28 201416:16:17
FRAC 0x92925552
memory type is W9751G6JB DDR2
Wait for ddr ready 1power 0x00820710
Frac 0x92925552
start change cpu freq
hbus 0x00000003
cpu 0x00010001
LLLLLLLFLCL0x8050100b
============================================================================
I read HW_RTC_PERSISTENT1_RD() in pwer_prep.c
============================================================================
pwer_prep.c
int _start( void )
{
int iRtn = SUCCESS;
printf("\r\n hylim 0 _start : HW_RTC_PERSISTENT1_RD = [0x%X]\x0d\x0a",HW_RTC_PERSISTENT1_RD());
#ifndef mx28
HW_DIGCTL_CTRL_SET(BM_DIGCTL_CTRL_USE_SERIAL_JTAG);
#else
#define SSP0_PIN_DRIVE_12mA 0x2
:
============================================================================
But both of them are different.
HW_RTC_PERSISTENT1_RD()
ERROR : 0x00000002
OK : 0x00000000
HW_RTC_PERSISTENT1_RD value is used in setup_cmdline_tag() function in /linux_prep/core/setup.c as " adding one to the rootfs partition number".
I know it is also related to 1.Kernel Panic problem.
And when I turn power on, I can see 0x80501003 before "HTLLLLLLL....."
It is also weird.
And unfortunately I couldn't use JTAG.
Please let me know any idea or advice.
Thanks,
Hi hongyup
error 0x80501003 means
//! The file signature or file version is incorrect.
So NAND is read incorrectly. Probably smth wrong
in power design, please find attached schematic for 5V only configuration.
You should follow it exactly, all capacitors values, Battery, DCDC_BATT
resistors should be placed as in attached schematic.
HW_RTC_PERSISTENT1_RD value shows PMU power state machine
(codes for each internal state): this also points that smth wrong with power-up.
I would suggest recheck with appnote below whole board power design
Using the i.MX28 Power Management Unit and Battery Charger: Getting Started with Power Supply
Also these errors may be caused by fact that you are powering on board when not its power
supplies (power capacitors) are fully discharged (<0.2V), if you are doing OFF-ON test many times.
Best regards
chip
Hi hongyup
schematic seems as correct.
These errors may be caused by fact that you are powering on board when not its power
supplies (power capacitors) are fully discharged (<0.2V), if you are doing OFF-ON test many times.
You should verify that VDD5V < 0.2V before chip will power-up again.
Best regards
chip
Hi Chip,
Thanks your kind reply.
I checked VDD5V < 0.2V before system power up.
But It is same(not work)
I'll check Power module again.
Anyway, Could you please let me know about "HW_RTC_PERSISTENT1_RD = [0x00000002]" in details?
How can HW_RTC_PERSISTENT1 register is changed by H/W or S/W?
Thanks agian,
hongyup
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.
For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )
Thank you for using Freescale Community.