Murata adapter for 1LV

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Murata adapter for 1LV

跳至解决方案
924 次查看
romitchatterjee
Contributor V

I want to evaluate Murata Type 1LV module with i.MX 6UL. Can I use Murata V1 and V2 adapters to connect 1LV to the i.MX 6UL?

标签 (2)
0 项奖励
回复
1 解答
783 次查看
bill_chen1
Contributor III

pastedImage_4.png

Fig1. i.MX 6UltraLite EVK with uSD-M.2 Adapter and Type 1LV M.2 EVB

pastedImage_2.png

Fig. 2: Murata uSD-M.2 adapter works with Embedded Artists’ 1LV EVB

Murata V1/V2 adapters are not recommended to evaluate Murata’s type 1LV module. Using Murata’s uSD-M.2 adapter and Embedded Artists’ 1LV M.2 EVB is a better solution for evaluating 1LV module on NXP’s i.MX6UL as Fig.1 shows. Note that 1LV can only work on 1.8V mode, so make sure to set uSD-M.2 adapter to 1.8V mode by removing the jumper on J12 as Fig.2 shows. Also, you need to build an image for i.MX6UL EVK for 1.8V mode. Murata’s build script provides options for you to build an image for i.MX 6UL on 1.8V. To learn more about the build script, please refer to Murata’s quick start guide here.

在原帖中查看解决方案

2 回复数
784 次查看
bill_chen1
Contributor III

pastedImage_4.png

Fig1. i.MX 6UltraLite EVK with uSD-M.2 Adapter and Type 1LV M.2 EVB

pastedImage_2.png

Fig. 2: Murata uSD-M.2 adapter works with Embedded Artists’ 1LV EVB

Murata V1/V2 adapters are not recommended to evaluate Murata’s type 1LV module. Using Murata’s uSD-M.2 adapter and Embedded Artists’ 1LV M.2 EVB is a better solution for evaluating 1LV module on NXP’s i.MX6UL as Fig.1 shows. Note that 1LV can only work on 1.8V mode, so make sure to set uSD-M.2 adapter to 1.8V mode by removing the jumper on J12 as Fig.2 shows. Also, you need to build an image for i.MX6UL EVK for 1.8V mode. Murata’s build script provides options for you to build an image for i.MX 6UL on 1.8V. To learn more about the build script, please refer to Murata’s quick start guide here.

783 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Romit Chatterjee,

It’s my understanding that Murata recommends using their newer solutions rather than the i.MX V1/V2 tool but you would need to check with them directly what support is still given to this adapter.

My apologies for the inconvenience!

Regards,

0 项奖励
回复