Dear All,
We are trying to test LBEE5HY1MW with our custom i.MX6ULL board.
Here is the setup:
Hardware:
(Attached[HW_Setup.JPEG] image for reference)
Software:
After successful build of backport drivers, trying to insmod the driver. But we are not getting wlan0 after registered new interface driver brcmfmac print.
As per Cypress community pages WiFi Firmware should load after registering brcmfmac and wlan0 interface should come up. But unfortunately we are not getting these prints.
All required firmware files are available in mentioned path (https://community.cypress.com/docs/DOC-14597) [/lib/firmware/brcm/]
To debug further on the issue, we tried to power Murata EVK through USB and tried configuring SDIO in-band interrupts. But still observing same issue.
Please help us to resolve this issue as soon as possible.
With Regards,
Keshava Kumar B
Hello Keshava,
I doubt the SDIO bus wiring can work the way you have implemented, especially for high speed. Perhaps you can try to lower the speed (~2 MHz) and see if that helps? The best way would be to have an M.2 interface on your board, of course, or at least an SD connector.